This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TAS5754M:3线I2S音频接口设置

Guru**** 2901510 points

Other Parts Discussed in Thread: TAS5754MDCAEVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/655862/tas5754m-3-wire-i2s-audio-interface-setting

部件号:TAS5754M

你(们)好  

1.使用  PurePath控制台2 GUI设置TAS5754MDCAEVM。

2.将MCLK (引脚22)连接至GND 或将MCLK (引脚22) 直接连接至SCLK (引脚23)

3.然后设置如下所示的寄存器值,该值可在E2E论坛中找到

TAS5754没有音频输出。   TAS5754不工作。

如何解决此问题?

谢谢

!3Wire模式
!无SCLK输入模式的系统时钟PLL模式。 提供电源电压(3.3V)。 暂时不提供I2S时钟。
! 通过I2C在地址=0x00处写入0x00。 (转至第0页)
X00 00 00
! 通过I2C在地址=0x02处写入0x10。 (待机请求)
X02 10.
! 通过I2C在地址=0x25处写入0x5A。 (忽略SCLK多路检测器,忽略SCLK检测,禁用自动分配器设置,忽略FS检测)
X25 5A
! 通过I2C在地址=0x0D处写入0x10。 (PLL时钟源=> BCLK)
X0D 10.
! 通过I2C在地址=0x14处写入0x00。 (P=1表示PLL分配器)
X14 00
! 通过I2C在地址=0x15处写入(对于BCLK=64fs,为0x10;对于BCLK=32fs,为0x20)请注意L&R 32位=32*2=64。 (对于PLL分配器,J=16/32)
X15 10.
! 通过I2C在地址=0x16处写入0x00。 (对于PLL分配器,D1=0)
X16 00
! 通过I2C在地址=0x17处写入0x00。 (对于PLL分配器,D2=0)
X17 00
! 通过I2C在地址=0x18处写入0x01。 (对于PLL分配器,R=2)
X18 01.
! 通过I2C在地址=0x1B处写入0x01。 (miniDSP CLK分配器= 2)
X1B 01
! 通过I2C在地址=0x1C处写入0x0F。 (DAC CLK分配器= 16)
X1C 0F
! 通过I2C在地址=0x1D处写入0x03。 (NCP CLK分禾器= 4)
X1D 03.
! 通过I2C在地址=0x1E处写入0x07。 (OSR CLK分配器= 8)
X1E 07.
! 通过I2C在地址=0x22处写入0x00。 (插值滤波器= 8x,FS设置= 48kHz)
x22 00
! 通过I2C在地址=0x23处写入0x04。 (IDAC = 1024个周期)
X23 04.
! 通过I2C在地址=0x24处写入0x00。 (IDAC = 1024个周期)
x24 00
! 通过I2C在地址=0x02处写入0x00。 (待机释放)
X02 00
! 提供I2S时钟(SCLK:连接至0,LRCLK:44.1kHz/48kHz,BCLK:32fs/64fs)