工具/软件:Linux
大家好,
我试图用TAS5733L替换运行Ubuntu 16.04 的ARTIK305中的ALC5658编码解码器。参考TI提供的编码解码器代码。我们还需要机器驱动程序吗? 或者编解码器代码足够用于TAS5733L集成。因为参考编解码器代码没有用于创建声卡的代码。
您是否有其他方法将 TAS5733L放大器与 运行Ubuntu 16.04 的ARTIK305集成在一起 (如果没有ALC5658编解码器)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:Linux
大家好,
我试图用TAS5733L替换运行Ubuntu 16.04 的ARTIK305中的ALC5658编码解码器。参考TI提供的编码解码器代码。我们还需要机器驱动程序吗? 或者编解码器代码足够用于TAS5733L集成。因为参考编解码器代码没有用于创建声卡的代码。
您是否有其他方法将 TAS5733L放大器与 运行Ubuntu 16.04 的ARTIK305集成在一起 (如果没有ALC5658编解码器)?
是的,对于立体声,我们得到的是0x2b。 我们能够检测到这一点。
[root@Artik ~]# i2ctect -y 1.
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -------- -------- ---
10:-------- -------- -------- --
20:-------- -------- -----------------
30:-------- -------- -------- --
40:-------- -------- -------- --
50:-------- -------- -------- --
60:-------- -------- -------- --
70:-------- ---
[root@Artik ~]#
即使我们按照您所说的那样设置值:
[ Gib] mmcblk1: mmc2:AAAA SL16G 14.8 3.94万
[ P2] mmcblk1:3.94.5万 P2.
[ 4.7.5万 ( 自动)]
5733 l 的"0级" reg 1b,值为0
[ 4.17.5万 ( 自动)]
5733 l 5的值为0
[ 4.17.5万 ( 自动)]
5733 l 的"0级"注册号为0
[ 4.17.5万 ( 自动)]
5733 l 的和平价为30
从处理器发出的I2S信号与屏幕截图连接良好。但我们无法在扬声器上听到任何声音。
请给出建议。
谢谢!
Nikhil