This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] [FAQ] TLV320AIC3120:动态更改TLV320AIC3120上的采样频率

Guru**** 2782575 points

Other Parts Discussed in Thread: TLV320AIC3120

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/773092/faq-tlv320aic3120-change-sampling-frequency-dynamically-on-the-tlv320aic3120

部件号:TLV320AIC3120

是否可以在TLV320AIC3120中动态/动态更改采样率?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    更改时钟设置时,假定为AIC3120。

    1)保持MCLK在当前采样率下运行。

    2)关闭ADC和DAC的电源。

    3)等待ADC和DAC加电标志清除(时间可能因软步进设置而异)。 这位于第0页,寄存器36和  37.

    4)关闭PLL

    5)如有必要,现在可以更改外部MCLK信号。

    6)如果编解码器是I2S主编解码器,请正确设置BCLK分配器。

    7)更改PLL设置并启动PLL。

    8)等待10ms,以便PLL锁定。

    9)设置时钟分频器值(例如 DOSR,MDAC,NDAC,AOSR,mAdc, NADC)以及miniDSP设置(即插值/小数因子)。

    10)根据需要为ADC和DAC加电。