This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] [FAQ]音频ADC/编解码器:如何处理TLV320ADC和TLV320AIC系列设备上未使用的输入?

Guru**** 2747375 points
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    TLV320ADC3100,TLV320ADC3101,TLV320ADC3001,TLV320AIC3203,TLV320AIC3253,TLV320AIC3204, TLV320AIC3254,TLV320AIC3206,TLV320AIC3256,TLV320AIC36,TLV320AIC3100, TLV320AIC3101,TLV320AIC3104,TLV320AIC3105,TLV320AIC3106,TLV320AIC3107, TLV320AIC3109,TLV320AIC3110,TLV320AIC3111,TLV320AIC3120,TLV320AIC3212, TLV320AIC3262,TLV320AIC3263和TLV320AIC3268

    对于TI的音频ADC和编解码器上未使用的输入,建议通过~0.47uF电容器提供至GND的交流端接,以防止非端接输入上的噪声拾取。   模拟输入上有直流偏压,因此不应直接与GND短路。  ~0.47uF电容器为器件内的直流偏置提供断路,但提供对GND的交流短路,以实现正确端接和降噪。