This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TAS5782M:TDM模式下的TAS5782,支持多通道

Guru**** 2798555 points

Other Parts Discussed in Thread: TAS5782M

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/771077/tas5782m-tas5782-in-tdm-mode-and-support-multi-channel

部件号:TAS5782M

我有几个项目,它们将支持5.1 .2ch和7.1 .4ch,

我使用6件TAS5782M进行设计,

现在,我没有声音输出。

我的情况如下:

MCLK 24.576MHz = 2个SCLK
SCLK 12.288MHz = 256*48
LRCLK 48K

寄存器0x28是0x13,32位,数据格式是DSP。

0x29是I2S位移。

是我错过了配置还是我需要检查问题,谢谢!

MCLK,SCLK对我来说是正确的,谢谢!