This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PCM3008:振荡器的频率稳定性

Guru**** 2867140 points

Other Parts Discussed in Thread: PCM3008

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1100119/pcm3008-frequency-stability-of-oscillator

部件号:PCM3008

您好,

通过将12.288MHz振荡器除以4获得的3.072MHz系统时钟(SYSCK)应用于PCM3008。
12.288MHz振荡器的频率稳定性是+/- 50ppm (标准值)。
是否建议将此振荡器与此规格一起用于PCM3008?

此致,
加藤