请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM48580 您好、Sirs、
根据数据表第5页、LM48580的输入电压(最大值)为3Vpp (~1.060Vrms)。
如果是5V VDD、它会损坏 LM48580器件、还是仅在输入电压超过3Vpp 时产生输出削波、因为绝对输入电压为 VDD+0.3V?
谢谢、此致、
陈耀恩
2021年7月20日
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.