我正在尝试使用 以下配置操作 TLV320AIC3101、并且很难确认我的寄存器是否设置正确。 是否有人可以查看我的设置并告诉我什么是错误的?
- 48kHz 采样率
- 无 PLL
- 来自 BCLK 的 CLKDIV_IN 源
- DAC FS/1
- MIC1RP/MIC1RM 至 DOUT 的麦克风输入
- 到 HPLOUT 和 HPROUT 的 DIN 输入
原理图如下:

我已进行硬件设置、在这里我将向 MIC1RP 和 MIC1RM 输入播放~400Hz 0.5Vpp 正弦波。 编解码器在正弦波上执行 AtoD、并通过 I2S 将其发送到主机 MCU。 MCU 回波 I2S 数据和编解码器并播放输出。 我可以听到耳机上的输出、但非常安静。 我尝试过几种不同的增益设置、但我不确定首先应该查看哪个增益设置。
以下是我的寄存器设置:
static const codecValues defaultRegisterMap[] = {
0x02, 0x00,
0x04, 0x04,
0x05, 0x00,
0x06, 0x00,
0x07, 0x0A, // 48 kHz fs, Left-DAC plays left channel input data, right-DAC plays right channel input data
0x08, 0x00,
0x09, 0x00,
0x0A, 0x00,
0x0B, 0x01,
0x0C, 0xF0, // Enable high pass filter for Left ADC and Right ADC
0x0D, 0x00,
0x0E, 0x80, // AC coupled high power output, psueo differential output
0x0F, 0x00, // Left ADC PGA gain of 0 dB
0x10, 0x3F, // Right ADC PGA gain of ~30 dB
0x11, 0xFF, // Disconnect MIC2L/R from left ADC
0x12, 0xFF, // Disconnect MIC2L/R from right ADC
0x13, 0x78, // Left ADC powered down. LINE1L not connected to left-ADC PGA. We only have input on the right ADC
0x14, 0x78, // Left Channel Analog Inputs to CM connection
0x15, 0xF8, // MIC1RP to Left-ADC Control Register. MIC1RP differential mode. LINE1R is not connected to left ADC.
0x16, 0x84, // MIC1RP to Right-ADC Control Register. Right ADC powered up, differential microphone mode, -0 DB volume
0x17, 0x78, // Right Channel Analog Inputs to CM Connection
0x18, 0xF8, // LINE1L not connected to right ADC
0x19, 0x80, // MIC bias selection. Disable bias = 0x00, AVDD is 0xC0, 0x40 is 2.0V, 0x80 is 2.5V
0x1A, 0x00, // Left-AGC control register
0x1B, 0x7F,
0x1C, 0x00,
0x1D, 0x00,
0x1E, 0x7F,
0x1F, 0x00,
0x20, 0x00,
0x21, 0x00,
0x22, 0x00,
0x23, 0x00,
0x24, 0x00,
0x25, 0xE0, // Left DAC powered up, Right DAC powered up, HPLCOM is independent single-ended output
0x26, 0x14, // HPRCOM is independent single-ended output, Short-Circuit Protection is enabled
0x28, 0x00,
0x29, 0xA0, // Left and right DAC output path selects path 2
0x2A, 0x38, // Output driver pop reduction
0x2B, 0x10, // Left-DAC digital volume control register
0x2C, 0x10, // Right-DAC Digital Volume Control Register
0x2E, 0x00, // PGA_R is NOT routed to HPLCOM
0x2F, 0x00, // DAC_L1 is NOT routed to HPROUT
0x31, 0x00,
0x32, 0x00,
0x33, 0x0D, // HPLOUT output level control to 0 dB.
0x35, 0x00,
0x36, 0x00,
0x38, 0x00,
0x39, 0x00,
0x3A, 0x0C, // HPLCOM Output level control register
0x3C, 0x00,
0x3D, 0x00,
0x3F, 0x00,
0x40, 0x00,
0x41, 0x0D, // HPROUT output level control to 0 dB.
0x43, 0x00, // PGA_L is NOT routed to HPROUT
0x44, 0x00,
0x46, 0x00,
0x47, 0x00,
0x48, 0x0C, // HPRCOM Output level control register
0x51, 0x00,
0x52, 0x00,
0x54, 0x00,
0x55, 0x00,
0x56, 0x00,
0x58, 0x00,
0x59, 0x00,
0x5B, 0x00,
0x5C, 0x00,
0x5D, 0x02,
0x5E, 0x00,
0x5F, 0x00,
0x65, 0x01,
0x66, 0xA2,
0x67, 0x00,
0x68, 0x00,
0x69, 0x00,
0x6A, 0x00,
0x6B, 0x00,
0x6C, 0x00,
0x6D, 0x00,
};
这是我尝试实现的音频路径:

如果我的设置有误、有人能告诉我吗?
谢谢。