This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TLV320ADC3101:需要建议将 TLV320ADC3101的直流失调电压降至零

Guru**** 2506915 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1010866/tlv320adc3101-need-suggestion-to-reduce-dc-offset-of-tlv320adc3101-to-zero

器件型号:TLV320ADC3101

您好、Sirs、

以下是  由 miniDSP 在 https://e2e.ti.com/support/audio-group/audio/f/audio-forum/929444/tlv320adc3101-dc-offset-questions-about-the-reason-impact-and-suggestion 线程上提供的直流块滤波器建议的内容

客户想知道我们是否可以优化页0x04配置、以将直流偏移降至零。 附加的文件是客户的0x04页设置以供参考。

------------------------------------------------------------------

0x30 - B0x00 (0)/ P0x04 (4)/ R0x0e (14)= 0x7f = 0111 1111 # 2
0x30 - B0x00 (0)/ P0x04 (4)/ R0x0f (15)= 0xa3 = 1010 0011 # 3
0x30 - B0x00 (0)/ P0x04 (4)/ R0x10 (16)= 0x80 = 1000 0000 # 4
0x30 - B0x00 (0)/P0x04 (4)/R0x11 (17)= 0x5d = 0101 1101 # 5
0x30 - B0x00 (0)/ P0x04 (4)/ R0x12 (18)= 0x7f = 0111 1111 # 6
0x30 - B0x00 (0)/ P0x04 (4)/ R0x13 (19)= 0xa3 = 1010 0011 # 7
0x30 - B0x00 (0)/ P0x04 (4)/ R0x14 (20)= 0x7f = 0111 1111 # 8
0x30 - B0x00 (0)/ P0x04 (4)/ R0x15 (21)= 0xa3 = 1010 0011 # 9
0x30 - B0x00 (0)/ P0x04 (4)/ R0x16 (22)= 0x80 = 1000 0000 #10
0x30 - B0x00 (0)/ P0x04 (4)/ R0x17 (23)= 0xba = 1011 1010 # 11
0x30 - B0x00 (0)/P0x04 (4)/R0x18 (24)= 0x7f = 0111 1111 # 12
0x30 - B0x00 (0)/ P0x04 (4)/ R0x19 (25)= 0xff = 1111 #13
0x30 - B0x00 (0)/ P0x04 (4)/ R0x1A (26)= 0x00 = 0000 # 14
0x30 - B0x00 (0)/ P0x04 (4)/ R0x1b (27)= 0x00 = 0000 # 15
0x30 - B0x00 (0)/ P0x04 (4)/ R0x1c (28)= 0x00 = 0000 0000 16
0x30 - B0x00 (0)/ P0x04 (4)/ R0x1d (29)= 0x00 = 0000 0000 #17
0x30 - B0x00 (0)/ P0x04 (4)/ R0x1e (30)= 0x00 = 0000 0000 18
0x30 - B0x00 (0)/ P0x04 (4)/ R0x1f (31)= 0x00 = 0000 0000 19
0x30 - B0x00 (0)/ P0x04 (4)/ R0x20 (32)= 0x00 = 0000 20
0x30 - B0x00 (0)/ P0x04 (4)/ R0x21 (33)= 0x00 = 0000 0000 21
0x30 - B0x00 (0)/ P0x04 (4)/ R0x22 (34)= 0x7f = 0111 1111 # 22
0x30 - B0x00 (0)/ P0x04 (4)/ R0x23 (35)= 0xff = 1111 # 23
0x30 - B0x00 (0)/ P0x04 (4)/ R0x24 (36)= 0x00 = 0000 # 24
0x30 - B0x00 (0)/ P0x04 (4)/ R0x25 (37)= 0x00 = 0000 # 25
0x30 - B0x00 (0)/ P0x04 (4)/ R0x26 (38)= 0x00 = 0000 # 26
0x30 - B0x00 (0)/ P0x04 (4)/ R0x27 (39)= 0x00 = 0000 #27
0x30 - B0x00 (0)/ P0x04 (4)/ R0x28 (40)= 0x00 = 0000 0000 28
0x30 - B0x00 (0)/ P0x04 (4)/ R0x29 (41)= 0x00 = 0000 # 29
0x30 - B0x00 (0)/ P0x04 (4)/ R0x2a (42)= 0x00 = 0000 # 30
0x30 - B0x00 (0)/ P0x04 (4)/ R0x2b (43)= 0x00 = 0000 # 31
0x30 - B0x00 (0)/P0x04 (4)/R0x2c (44)= 0x7f = 0111 1111 # 32
0x30 - B0x00 (0)/ P0x04 (4)/ R0x2d (45)= 0xff = 1111 # 33
0x30 - B0x00 (0)/ P0x04 (4)/ R0x2e (46)= 0x00 = 0000 # 34
0x30 - B0x00 (0)/ P0x04 (4)/ R0x2f (47)= 0x00 = 0000 0000 #35
0x30 - B0x00 (0)/ P0x04 (4)/ R0x30 (48)= 0x00 = 0000 # 36
0x30 - B0x00 (0)/ P0x04 (4)/ R0x31 (49)= 0x00 = 0000 #37
0x30 - B0x00 (0)/ P0x04 (4)/ R0x32 (50)= 0x00 = 0000 # 38
0x30 - B0x00 (0)/ P0x04 (4)/ R0x33 (51)= 0x00 = 0000 # 39
0x30 - B0x00 (0)/ P0x04 (4)/ R0x34 (52)= 0x00 = 0000 # 40
0x30 - B0x00 (0)/ P0x04 (4)/ R0x35 (53)= 0x00 = 0000 # 41
0x30 - B0x00 (0)/P0x04 (4)/R0x36 (54)= 0x7f = 0111 1111 # 42
0x30 - B0x00 (0)/ P0x04 (4)/ R0x37 (55)= 0xff = 1111 #43
0x30 - B0x00 (0)/P0x04 (4)/R0x38 (56)= 0x00 = 0000 #44
0x30 - B0x00 (0)/ P0x04 (4)/ R0x39 (57)= 0x00 = 0000 # 45
0x30 - B0x00 (0)/ P0x04 (4)/ R0x3a (58)= 0x00 = 0000 0000 #46
0x30 - B0x00 (0)/ P0x04 (4)/ R0x3b (59)= 0x00 = 0000 0000 47
0x30 - B0x00 (0)/ P0x04 (4)/ R0x3c (60)= 0x00 = 0000 0000 48
0x30 - B0x00 (0)/P0x04 (4)/R0x3d (61)= 0x00 = 0000 # 49
0x30 - B0x00 (0)/ P0x04 (4)/ R0x3E (62)= 0x00 = 0000 0000 50
0x30 - B0x00 (0)/ P0x04 (4)/ R0x3f (63)= 0x00 = 0000 0000 #51
0x30 - B0x00 (0)/ P0x04 (4)/ R0x4e (78)= 0x7f = 0111 1111 # 52
0x30 - B0x00 (0)/ P0x04 (4)/ R0x4f (79)= 0xa3 = 1010 0011 # 53
0x30 - B0x00 (0)/P0x04 (4)/R0x50 (80)= 0x80 = 1000 0000 #54
0x30 - B0x00 (0)/P0x04 (4)/R0x51 (81)= 0x5d = 0101 1101 # 55
0x30 - B0x00 (0)/P0x04 (4)/R0x52 (82)= 0x7f = 0111 1111 # 56
0x30 - B0x00 (0)/ P0x04 (4)/ R0x53 (83)= 0xa3 = 1010 0011 # 57
0x30 - B0x00 (0)/P0x04 (4)/R0x54 (84)= 0x7f = 0111 1111 # 58
0x30 - B0x00 (0)/ P0x04 (4)/ R0x55 (85)= 0xa3 = 1010 0011 # 59
0x30 - B0x00 (0)/ P0x04 (4)/ R0x56 (86)= 0x80 = 1000 0000 # 60
0x30 - B0x00 (0)/P0x04 (4)/R0x57 (87)= 0xba = 1011 1010 # 61
0x30 - B0x00 (0)/P0x04 (4)/R0x58 (88)= 0x7f = 0111 1111 # 62
0x30 - B0x00 (0)/ P0x04 (4)/ R0x59 (89)= 0xff = 1111 #63
0x30 - B0x00 (0)/ P0x04 (4)/ R0x5a (90)= 0x00 = 0000 0000 64
0x30 - B0x00 (0)/ P0x04 (4)/ R0x5b (91)= 0x00 = 0000 0000 #65
0x30 - B0x00 (0)/ P0x04 (4)/ R0x5c (92)= 0x00 = 0000 0000 #66
0x30 - B0x00 (0)/ P0x04 (4)/ R0x5d (93)= 0x00 = 0000 0000 #67
0x30 - B0x00 (0)/ P0x04 (4)/ R0x5e (94)= 0x00 = 0000 0000 #68
0x30 - B0x00 (0)/ P0x04 (4)/ R0x5f (95)= 0x00 = 0000 0000 #69
0x30 - B0x00 (0)/ P0x04 (4)/ R0x60 (96)= 0x00 = 0000 0000 70
0x30 - B0x00 (0)/ P0x04 (4)/ R0x61 (97)= 0x00 = 0000 0000 71
0x30 - B0x00 (0)/P0x04 (4)/R0x62 (98)= 0x7f = 0111 1111 # 72
0x30 - B0x00 (0)/ P0x04 (4)/ R0x63 (99)= 0xff = 1111 # 73
0x30 - B0x00 (0)/ P0x04 (4)/ R0x64 (100)= 0x00 = 0000 # 74
0x30 - B0x00 (0)/ P0x04 (4)/ R0x65 (101)= 0x00 = 0000 0000 75
0x30 - B0x00 (0)/ P0x04 (4)/ R0x66 (102)= 0x00 = 0000 0000 #76
0x30 - B0x00 (0)/ P0x04 (4)/ R0x67 (103)= 0x00 = 0000 0000 #77
0x30 - B0x00 (0)/ P0x04 (4)/ R0x68 (104)= 0x00 = 0000 0000 #78
0x30 - B0x00 (0)/ P0x04 (4)/ R0x69 (105)= 0x00 = 0000 0000 79
0x30 - B0x00 (0)/ P0x04 (4)/ R0x6a (106)= 0x00 = 0000 0000 80
0x30 - B0x00 (0)/ P0x04 (4)/ R0x6b (107)= 0x00 = 0000 0000 #81
0x30 - B0x00 (0)/ P0x04 (4)/ R0x6c (108)= 0x7f = 0111 1111 # 82
0x30 - B0x00 (0)/ P0x04 (4)/ R0x6d (109)= 0xff = 1111 #83
0x30 - B0x00 (0)/ P0x04 (4)/ R0x6e (110)= 0x00 = 0000 0000 84
0x30 - B0x00 (0)/ P0x04 (4)/ R0x6f (111)= 0x00 = 0000 0000 #85
0x30 - B0x00 (0)/ P0x04 (4)/ R0x70 (112)= 0x00 = 0000 0000 86
0x30 - B0x00 (0)/P0x04 (4)/R0x71 (113)= 0x00 = 0000 #87
0x30 - B0x00 (0)/ P0x04 (4)/ R0x72 (114)= 0x00 = 0000 0000 #88
0x30 - B0x00 (0)/ P0x04 (4)/ R0x73 (115)= 0x00 = 0000 0000 89
0x30 - B0x00 (0)/ P0x04 (4)/ R0x74 (116)= 0x00 = 0000 0000 90
0x30 - B0x00 (0)/ P0x04 (4)/ R0x75 (117)= 0x00 = 0000 0000 91
0x30 - B0x00 (0)/P0x04 (4)/R0x76 (118)= 0x7f = 0111 1111 # 92
0x30 - B0x00 (0)/ P0x04 (4)/ R0x77 (119)= 0xff = 1111 #93
0x30 - B0x00 (0)/ P0x04 (4)/ R0x78 (120)= 0x00 = 0000 0000 94
0x30 - B0x00 (0)/ P0x04 (4)/ R0x79 (121)= 0x00 = 0000 0000 #95
0x30 - B0x00 (0)/ P0x04 (4)/ R0x7a (122)= 0x00 = 0000 0000 #96
0x30 - B0x00 (0)/ P0x04 (4)/ R0x7b (123)= 0x00 = 0000 0000 #97
0x30 - B0x00 (0)/ P0x04 (4)/ R0x7c (124)= 0x00 = 0000 0000 98
0x30 - B0x00 (0)/ P0x04 (4)/ R0x7d (125)= 0x00 = 0000 0000 #99
0x30 - B0x00 (0)/ P0x04 (4)/ R0x7e (126)= 0x00 = 0000 0000 100
0x30 - B0x00 (0)/ P0x04 (4)/ R0x7f (127)= 0x00 = 0000 0000 101

0x32 - B0x00 (0)/ P0x04 (4)/ R0x0e (14)= 0x7f = 0111 1111 # 104
0x32 - B0x00 (0)/ P0x04 (4)/ R0x0f (15)= 0xa3 = 1010 0011 # 105
0x32 - B0x00 (0)/ P0x04 (4)/ R0x10 (16)= 0x80 = 1000 0000 #106
0x32 - B0x00 (0)/P0x04 (4)/R0x11 (17)= 0x5d = 0101 1101 # 107
0x32 - B0x00 (0)/P0x04 (4)/R0x12 (18)= 0x7f = 0111 1111 # 108
0x32 - B0x00 (0)/ P0x04 (4)/ R0x13 (19)= 0xa3 = 1010 0011 # 109
0x32 - B0x00 (0)/ P0x04 (4)/ R0x14 (20)= 0x7f = 0111 1111 # 110
0x32 - B0x00 (0)/ P0x04 (4)/ R0x15 (21)= 0xa3 = 1010 0011 # 111
0x32 - B0x00 (0)/ P0x04 (4)/ R0x16 (22)= 0x80 = 1000 0000 #112
0x32 - B0x00 (0)/ P0x04 (4)/ R0x17 (23)= 0xba = 1011 1010 # 113
0x32 - B0x00 (0)/P0x04 (4)/R0x18 (24)= 0x7f = 0111 1111 # 114
0x32 - B0x00 (0)/ P0x04 (4)/ R0x19 (25)= 0xff = 1111 # 115
0x32 - B0x00 (0)/ P0x04 (4)/ R0x1A (26)= 0x00 = 0000 0000 116
0x32 - B0x00 (0)/P0x04 (4)/R0x1b (27)= 0x00 = 0000 #117
0x32 - B0x00 (0)/ P0x04 (4)/ R0x1c (28)= 0x00 = 0000 0000 118
0x32 - B0x00 (0)/ P0x04 (4)/ R0x1d (29)= 0x00 = 0000 0000 #119
0x32 - B0x00 (0)/ P0x04 (4)/ R0x1e (30)= 0x00 = 0000 # 120
0x32 - B0x00 (0)/ P0x04 (4)/ R0x1f (31)= 0x00 = 0000 0000 121
0x32 - B0x00 (0)/ P0x04 (4)/ R0x20 (32)= 0x00 = 0000 #122
0x32 - B0x00 (0)/ P0x04 (4)/ R0x21 (33)= 0x00 = 0000 #123
0x32 - B0x00 (0)/ P0x04 (4)/ R0x22 (34)= 0x7f = 0111 1111 # 124
0x32 - B0x00 (0)/ P0x04 (4)/ R0x23 (35)= 0xff = 1111 #125
0x32 - B0x00 (0)/ P0x04 (4)/ R0x24 (36)= 0x00 = 0000 # 126
0x32 - B0x00 (0)/ P0x04 (4)/ R0x25 (37)= 0x00 = 0000 #127
0x32 - B0x00 (0)/ P0x04 (4)/ R0x26 (38)= 0x00 = 0000 # 128
0x32 - B0x00 (0)/ P0x04 (4)/ R0x27 (39)= 0x00 = 0000 #129
0x32 - B0x00 (0)/ P0x04 (4)/ R0x28 (40)= 0x00 = 0000 #130
0x32 - B0x00 (0)/ P0x04 (4)/ R0x29 (41)= 0x00 = 0000 #131
0x32 - B0x00 (0)/ P0x04 (4)/ R0x2a (42)= 0x00 = 0000 0000 132
0x32 - B0x00 (0)/ P0x04 (4)/ R0x2b (43)= 0x00 = 0000 #133
0x32 - B0x00 (0)/P0x04 (4)/R0x2c (44)= 0x7f = 0111 1111 # 134
0x32 - B0x00 (0)/ P0x04 (4)/ R0x2d (45)= 0xff = 1111 #135
0x32 - B0x00 (0)/ P0x04 (4)/ R0x2e (46)= 0x00 = 0000 # 136
0x32 - B0x00 (0)/ P0x04 (4)/ R0x2f (47)= 0x00 = 0000 0000 #137
0x32 - B0x00 (0)/ P0x04 (4)/ R0x30 (48)= 0x00 = 0000 #138
0x32 - B0x00 (0)/ P0x04 (4)/ R0x31 (49)= 0x00 = 0000 0000 139
0x32 - B0x00 (0)/ P0x04 (4)/ R0x32 (50)= 0x00 = 0000 # 140
0x32 - B0x00 (0)/ P0x04 (4)/ R0x33 (51)= 0x00 = 0000 0000 141
0x32 - B0x00 (0)/ P0x04 (4)/ R0x34 (52)= 0x00 = 0000 # 142
0x32 - B0x00 (0)/ P0x04 (4)/ R0x35 (53)= 0x00 = 0000 #143
0x32 - B0x00 (0)/P0x04 (4)/R0x36 (54)= 0x7f = 0111 1111 # 144
0x32 - B0x00 (0)/ P0x04 (4)/ R0x37 (55)= 0xff = 1111 # 145
0x32 - B0x00 (0)/P0x04 (4)/R0x38 (56)= 0x00 = 0000 # 146
0x32 - B0x00 (0)/ P0x04 (4)/ R0x39 (57)= 0x00 = 0000 #147
0x32 - B0x00 (0)/ P0x04 (4)/ R0x3a (58)= 0x00 = 0000 0000 148
0x32 - B0x00 (0)/ P0x04 (4)/ R0x3b (59)= 0x00 = 0000 0000 #149
0x32 - B0x00 (0)/ P0x04 (4)/ R0x3c (60)= 0x00 = 0000 0000 #150
0x32 - B0x00 (0)/ P0x04 (4)/ R0x3d (61)= 0x00 = 0000 # 151
0x32 - B0x00 (0)/ P0x04 (4)/ R0x3E (62)= 0x00 = 0000 0000 152
0x32 - B0x00 (0)/P0x04 (4)/R0x3f (63)= 0x00 = 0000 # 153
0x32 - B0x00 (0)/ P0x04 (4)/ R0x4e (78)= 0x7f = 0111 1111 # 154
0x32 - B0x00 (0)/ P0x04 (4)/ R0x4f (79)= 0xa3 = 1010 0011 # 155
0x32 - B0x00 (0)/ P0x04 (4)/ R0x50 (80)= 0x80 = 1000 0000 # 156
0x32 - B0x00 (0)/P0x04 (4)/R0x51 (81)= 0x5d = 0101 1101 # 157
0x32 - B0x00 (0)/P0x04 (4)/R0x52 (82)= 0x7f = 0111 1111 # 158
0x32 - B0x00 (0)/ P0x04 (4)/ R0x53 (83)= 0xa3 = 1010 0011 # 159
0x32 - B0x00 (0)/P0x04 (4)/R0x54 (84)= 0x7f = 0111 1111 # 160
0x32 - B0x00 (0)/ P0x04 (4)/ R0x55 (85)= 0xa3 = 1010 0011 # 161
0x32 - B0x00 (0)/ P0x04 (4)/ R0x56 (86)= 0x80 = 1000 0000 162
0x32 - B0x00 (0)/P0x04 (4)/R0x57 (87)= 0xba = 1011 1010 # 163
0x32 - B0x00 (0)/P0x04 (4)/R0x58 (88)= 0x7f = 0111 1111 # 164
0x32 - B0x00 (0)/ P0x04 (4)/ R0x59 (89)= 0xff = 1111 # 165
0x32 - B0x00 (0)/ P0x04 (4)/ R0x5a (90)= 0x00 = 0000 0000 166
0x32 - B0x00 (0)/ P0x04 (4)/ R0x5b (91)= 0x00 = 0000 0000 167
0x32 - B0x00 (0)/ P0x04 (4)/ R0x5c (92)= 0x00 = 0000 0000 168
0x32 - B0x00 (0)/P0x04 (4)/R0x5d (93)= 0x00 = 0000 0000 169
0x32 - B0x00 (0)/ P0x04 (4)/ R0x5e (94)= 0x00 = 0000 0000 #170
0x32 - B0x00 (0)/ P0x04 (4)/ R0x5f (95)= 0x00 = 0000 0000 171
0x32 - B0x00 (0)/P0x04 (4)/R0x60 (96)= 0x00 = 0000编号172
0x32 - B0x00 (0)/ P0x04 (4)/ R0x61 (97)= 0x00 = 0000 #173
0x32 - B0x00 (0)/P0x04 (4)/R0x62 (98)= 0x7f = 0111 1111 # 174
0x32 - B0x00 (0)/P0x04 (4)/R0x63 (99)= 0xff = 1111 #175
0x32 - B0x00 (0)/ P0x04 (4)/ R0x64 (100)= 0x00 = 0000 # 176
0x32 - B0x00 (0)/ P0x04 (4)/ R0x65 (101)= 0x00 = 0000 #177
0x32 - B0x00 (0)/ P0x04 (4)/ R0x66 (102)= 0x00 = 0000 0000 178
0x32 - B0x00 (0)/P0x04 (4)/R0x67 (103)= 0x00 = 0000 # 179
0x32 - B0x00 (0)/ P0x04 (4)/ R0x68 (104)= 0x00 = 0000 0000 180
0x32 - B0x00 (0)/ P0x04 (4)/ R0x69 (105)= 0x00 = 0000 # 181
0x32 - B0x00 (0)/ P0x04 (4)/ R0x6a (106)= 0x00 = 0000 0000 182
0x32 - B0x00 (0)/ P0x04 (4)/ R0x6b (107)= 0x00 = 0000 # 183
0x32 - B0x00 (0)/ P0x04 (4)/ R0x6c (108)= 0x7f = 0111 1111 # 184
0x32 - B0x00 (0)/ P0x04 (4)/ R0x6d (109)= 0xff = 1111 # 185
0x32 - B0x00 (0)/ P0x04 (4)/ R0x6e (110)= 0x00 = 0000 0000 186.
0x32 - B0x00 (0)/ P0x04 (4)/ R0x6f (111)= 0x00 = 0000 0000 #187
0x32 - B0x00 (0)/ P0x04 (4)/ R0x70 (112)= 0x00 = 0000 #188
0x32 - B0x00 (0)/ P0x04 (4)/ R0x71 (113)= 0x00 = 0000 0000 189
0x32 - B0x00 (0)/ P0x04 (4)/ R0x72 (114)= 0x00 = 0000 0000 #190
0x32 - B0x00 (0)/P0x04 (4)/R0x73 (115)= 0x00 = 0000 # 191
0x32 - B0x00 (0)/ P0x04 (4)/ R0x74 (116)= 0x00 = 0000 # 192
0x32 - B0x00 (0)/P0x04 (4)/R0x75 (117)= 0x00 = 0000 #193
0x32 - B0x00 (0)/P0x04 (4)/R0x76 (118)= 0x7f = 0111 1111 # 194
0x32 - B0x00 (0)/ P0x04 (4)/ R0x77 (119)= 0xff = 1111 #195
0x32 - B0x00 (0)/ P0x04 (4)/ R0x78 (120)= 0x00 = 0000 # 196
0x32 - B0x00 (0)/P0x04 (4)/R0x79 (121)= 0x00 = 0000 # 197
0x32 - B0x00 (0)/ P0x04 (4)/ R0x7a (122)= 0x00 = 0000 0000 #198
0x32 - B0x00 (0)/ P0x04 (4)/ R0x7b (123)= 0x00 = 0000 0000 #199
0x32 - B0x00 (0)/ P0x04 (4)/ R0x7c (124)= 0x00 = 0000 0000 #200
0x32 - B0x00 (0)/ P0x04 (4)/ R0x7d (125)= 0x00 = 0000 0000 #201
0x32 - B0x00 (0)/ P0x04 (4)/ R0x7e (126)= 0x00 = 0000 0000 #202
0x32 - B0x00 (0)/ P0x04 (4)/ R0x7f (127)= 0x00 = 0000 0000 #203
------------------------------------------------------------------

谢谢、此致、

陈耀恩
2021年6月18日

e2e.ti.com/.../tlv320_5F00_dc_5F00_offset_5F00_param.cfge2e.ti.com/.../tlv320_5F00_dc_5F00_offset_5F00_param_2D00_Memory.txt

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Wayne、

    在我看来、每个器件的左右通道仅使用双二阶1、而其他滤波器设置为默认值。 根据您提供的系数、下面是双二阶1的响应:

    这是所需的滤波器响应吗? 如果您想去除数据中的直流分量、则需要在其他两个比额表中的一个中实现高通滤波器。

    最棒的

    Zak

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的建议、Zak。 我们建议客户添加高通滤波器以移除直流偏移组件...Wayne Chen

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Zak 您好!

    此外、我们能否使用第1页的抖动控制寄存器寄存器26来校准客户 ADC3110器件的直流偏移?
     


    谢谢、此致、

    陈耀恩
    2021年6月25日


  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Wayne、

    是的、但更有可能的是、该抖动寄存器没有校准您所看到偏移的分辨率、因为它只能以+/-15mV 的阶跃进行设置、这可能已经大于您需要校准的直流偏移。

    最棒的

    Zak

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的建议、Zak...Wayne Chen

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Wayne、

    我对不同的滤波器选项进行了一些测试、以消除直流组件。 我发现最好将可编程 IIR 滤波器用作 HPF。 随附的是我的测试结果:

    e2e.ti.com/.../TLV320ADC3100-Idle-Tones.pptx

    请注意、这还讨论了差分输入的空闲音调以及高通滤波器选项。

    最棒的

    Zak

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Zak、您好、感谢您的详细回答... Wayne Chen