请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TAS5411-Q1 大家好、
只需确认一件事情:
如果客户希望使用5V 电源驱动4欧姆8w 扬声器、这还不够、对吧?
BTL:P=up^2/(2R)=(Vcc)^2/(2R)=Vcc^2/(2R)=5*5/(2*4)=3.5W
为了实现8W 4欧姆、至少需要8V 电源、对吧?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、
只需确认一件事情:
如果客户希望使用5V 电源驱动4欧姆8w 扬声器、这还不够、对吧?
BTL:P=up^2/(2R)=(Vcc)^2/(2R)=Vcc^2/(2R)=5*5/(2*4)=3.5W
为了实现8W 4欧姆、至少需要8V 电源、对吧?
谢谢!