请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPA2011D11、您能否共享最佳的 TI 解决方案而不是 ALC1003-VB-CGT?
2、您能否分享满足以下最新客户要求的最佳解决方案。
这些插座与客户的插座相同。
[要求]
规格:5V calss-D (需要驱动高达8Ω Ω、1W)
电压:3.3-5V
应用程序:非汽车
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.