请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPA3223 在数据流中、四个自举电容器的理想值通常为33nF、而图10.6和10.1显示220nF。 评估模块也使用33nF。 就效率而言、220nF 似乎很关键、尤其是 PVDD 小于30V 时。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在数据流中、四个自举电容器的理想值通常为33nF、而图10.6和10.1显示220nF。 评估模块也使用33nF。 就效率而言、220nF 似乎很关键、尤其是 PVDD 小于30V 时。