This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TLV320ADC3120:TLV320ADC3120寄存器配置表

Guru**** 2826755 points

Other Parts Discussed in Thread: TLV320ADC3120

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1335978/tlv320adc3120-tlv320adc3120-register-configurations-table

器件型号:TLV320ADC3120

大家好、

需要提供 TLV320ADC3120寄存器配置表。

TLV320ADC3120需要配置为 I2S 从器件2通道16位8kHz 采样率的输出。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Kevin:

    附件是符合您要求的基本配置、但我建议为此器件下载 PurePath 控制台3并针对您的用例进行配置、然后可以在 End System Integration 选项卡中将转储寄存到.cfg 文件中。

    # CHECKSUM 0
    # Generated by ADCx120EVM-SW v3.0.5
    # TLV320ADC3120 device configuration
    # -----------------------------------------------------------------------------
    # Reset
    # -----------------------------------------------------------------------------
    # Select Page 0
    w 98 00 00
    # Reset Device
    w 98 01 01
    # 1mS Delay
    # -----------------------------------------------------------------------------
    # Begin Device Memory
    # -----------------------------------------------------------------------------
    # Page 0 (0x00) Dump
    # Select Page 0
    w 98 00 00
    # Wake up and Enable AREG
    w 98 02 81
    w 98 05 01
    # ASI configuration
    w 98 07 40
    # ASI Channel configuration
    w 98 0c 00
    w 98 0d 00
    w 98 0e 00
    # ASI master mode
    w 98 13 00
    # PDM Configuration
    w 98 1f 08
    # Channel 1 configuration
    w 98 3c 04
    # Channel 2 configuration
    w 98 41 04
    # DSP Configuration
    w 98 6c 48
    # input and output Configuration
    w 98 74 f0
    # Page 1 (0x01) Dump
    # Select Page 1
    w 98 00 01
    #VAD configurations
    w 98 1e 00
    w 98 1f 00
    
    

    此致、