This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TAS2505:AM6234:播放:PCM_WRITE:2146:写入错误:输入/输出错误

Guru**** 2604035 points
Other Parts Discussed in Thread: TAS2505

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1454928/tas2505-am6234-aplay-pcm_write-2146-write-error-input-output-error

器件型号:TAS2505

工具与软件:

尊敬的 TI:

当我使用"Aplay"命令进行音频驱动程序测试时、将报告以下错误:

root@tiny:~# aplay sample-3s.wav
Playing WAVE 'sample-3s.wav' : [   25.317396] tas2505-codec 2-0018: tas2505_hw_params: bit width = 16
Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
[   25.347392] davinci-mcasp 2b10000.audio-controller: Sample-rate is off by 400 PPM
[   25.357478] tas2505-codec 2-0018: tas2505_set_bias_level:power on
aplay: pcm_write:2146: write error: Input/output error
[   45.737567] tas2505-codec 2-0018: tas2505_set_bias_level:SND_SOC_BIAS_STANDBY
[   45.747864] tas2505-codec 2-0018: tas2505_set_bias_level:power off
root@tiny:~#

tas2505的驱动程序来自以下链接: https://git.ti.com/cgit/lpaa-android-drivers/tas2505-linux-driver/ 、设备树配置也基于此链接进行配置。 但是 "CLK_McASP" 具有一个实例 "启用 GPIO" 节点、因此未对其进行配置。

/{	
	clk_mcasp1_fixed: clk_mcasp1_fixed {
		#clock-cells = <0>;
		compatible = "fixed-clock";
		clock-frequency = <24576000>;
	};

	clk_mcasp1: clk_mcasp1 {
		#clock-cells = <0>;
		compatible = "gpio-gate-clock";
		clocks = <&clk_mcasp1_fixed>;
		//enable-gpios = <&gpio1 27 0>; /* BeagleBone Black Clk enable on GPIO1_27 */
	};

	codec_audio: sound {
		compatible = "simple-audio-card";
		simple-audio-card,name = "AM62x-SKEVM";
		simple-audio-card,dai-link@0 {
			format = "i2s";
			bitclock-master = <&sound0_master>;
			frame-master = <&sound0_master>;
			sound0_master: cpu {
				sound-dai = <&mcasp1>;
				clocks = <&clk_mcasp1>;
			};

			codec {
				sound-dai = <&tas2505>;
			};
		};
	};
};

由于 'enable-gopios' 未配置节点、引导日志将出现以下错误:

[    0.813168] clk_mcasp1: gpio_clk_driver_probe: Can't get 'enable' named GPIO property
[    0.821220] gpio-clk: probe of clk_mcasp1 failed with error -2

我想问的是、出现错误消息的原因是什么 "播放:PCM_WRITE:2146:写入错误:输入/输出错误" ? 与节点有关 'ENABLE-GPIOs' 未配置? 如果相关、您能告诉我如何配置 'enable-gopios' 节点?

声卡信息和设备节点信息如下:

root@tiny:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: AM62xSKEVM [AM62x-SKEVM], device 0: davinci-mcasp.0-tas2505-hifi tas2505-hifi-0 [davinci-mcasp.0-tas2505-hifi tas2505-hifi-0]
  Subdevices: 1/1
  Subdevice #0: subdevice #0
root@tiny:~# cat /proc/asound/
AM62xSKEVM/  card0/       cards        devices      pcm          timers       version
root@tiny:~# cat /proc/asound/cards
 0 [AM62xSKEVM     ]: simple-card - AM62x-SKEVM
                      AM62x-SKEVM
root@tiny:~# ls /dev/snd/
controlC0  pcmC0D0p   timer
root@tiny:~#