This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TLV320AIC3110:TLV320AIC3110

Guru**** 2589300 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1480044/tlv320aic3110-tlv320aic3110

器件型号:TLV320AIC3110

工具与软件:

尊敬的先生:

I2C 主器件现在在我们的定制板上正常工作。 我们需要在记录模式下使用编解码器 I2C 配置脚本。 您能提供吗?

此致、

Samudralankaiah

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Samudralankaiah:

    这是 EVM 提供的一个参考脚本。 它包含录音设置。

    #			--------------------------------------------------------------- page 0 is selected 
    w 30 00 00
    #			 s/w reset
    > 01
    #			 PLL_clkin = BCLK,codec_clkin = PLL_CLK
    w 30 04 07
    > 91
    > 20
    > 00
    > 00
    #			 mode is i2s,wordlength is 16
    w 30 1b 00
    #			 NDAC is powered up and set to 4
    w 30 0b 84
    #			 MDAC is powered up and set to 4
    > 84
    w 30 12 84
    > 84
    #			 DOSR = 128, DOSR(9:8) = 0
    > 00
    #			             DOSR(7:0) = 128
    > 80
    #			 DAC => volume control thru pin disable 
    w 30 74 00
    #			 DAC => drc disable, th and hy
    w 30 44 00
    #			 DAC => 0 db gain left
    w 30 41 00
    #			 DAC => 0 db gain right
    > 00
    #			--------------------------------------------------------------- page 1 is selected
    w 30 00 01
    #			 De-pop, Power on = 800 ms, Step time = 4 ms
    w 30 21 4e
    #			 HPL and HPR powered up
    w 30 1f c2
    #			 LDAC routed to HPL, RDAC routed to HPR
    w 30 23 44
    #			 HPL unmute and gain 1db
    w 30 28 0e
    #			 HPR unmute and gain 1db
    > 0e
    #			 No attenuation on HP
    w 30 24 00
    w 30 25 00
    
    #			 MIC BIAS = AVDD
    w 30 2e 0b
    #			 MICPGA P = MIC 10k
    w 30 30 40
    #			 MICPGA M - CM 10k
    > 40
    #			--------------------------------------------------------------- page 0 is selected
    w 30 00 00
    #			 select DAC DSP mode 11 & enable adaptive filter
    w 30 3c 0b
    w 30 00 08
    w 30 01 04
    w 30 00 00
    #			 POWERUP DAC left and right channels (soft step disable)
    w 30 3f d6
    #			 UNMUTE DAC left and right channels
    > 00
    #			 POWERUP ADC channel
    w 30 51 80
    #			 UNMUTE ADC channel
    > 00
    #			--------------------------------------------------------------- page 1 is selected
    w 30 00 01
    #			 Unmute Class-D Left
    w 30 2a 1c
    #			 Unmute Class-D Right
    w 30 2b 1c
    #			 Power-up Class-D drivers
    w 30 20 c6

    此致、
    Jeff McPherson