This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LP-EM-CC2340R53:[BLE 6.0 CS DKC]通过 BLE 消息队列将外部数据传输到 BLE 栈

Guru**** 2924060 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1537996/lp-em-cc2340r53-ble-6-0-cs-dkc-transmitting-external-data-to-ble-stack-via-ble-message-queue

器件型号:LP-EM-CC2340R53


工具/软件:

您好、TI

*SDK 版本:9.11.00.18、示例: key_node

我们需要通过蓝牙传输按键事件。 为了实现这一点、我修改了  密钥中断回调函数  可将密钥数据转发到  BLE 堆栈  流经  BLE 消息队列

void BLE_button_event(uint32_t event, GapAdv_data_t *pBuf, uint32_t arg)
{
    BLEAppUtil_AdvEventData_t *pData = BLEAppUtil_malloc(sizeof(BLEAppUtil_AdvEventData_t));

    if (pData != NULL)
    {
        pData->event = event;
        pData->pBuf = pBuf;
        pData->arg = &arg;

        // Enqueue the event
        if (BLEAppUtil_enqueueMsg(BLEAPPUTIL_EVT_ADV_CB_EVENT, pData) != SUCCESS)
        {
            if (pBuf != NULL)
            {
                BLEAppUtil_free(pBuf);
            }
            BLEAppUtil_free(pData);
        }
    }
    else
    {
        if (pBuf != NULL)
        {
            BLEAppUtil_free(pBuf);
        }
    }
}

void App_ButtonCallBack(uint32_t events, uint32_t button_id)  /*IN: Events from keyboard module  */
{
    BLE_button_event(events, NULL, button_id);
}

/*
 *  ======== handleButtonCallback ========
 */
void handleButtonCallback(Button_Handle handle, Button_EventMask events)
{
    if (Button_EV_CLICKED == (events & Button_EV_CLICKED))
    {
        if(handle == buttonHandle[CONFIG_BUTTON_0])
        {
            button_num = 0x00;
            App_ButtonCallBack(BLEAPPUTIL_BUTTON_CLICK, button_num);
        }
        else if(handle == buttonHandle[CONFIG_BUTTON_1])
        {
            button_num = 0x01;
            App_ButtonCallBack(BLEAPPUTIL_BUTTON_CLICK, button_num);
        }
        else
        {}
    }
}

我在 Peripheral_Adv EventHandler 中接收并打印按键数据、但发现收到的 advMsg->arg 有时与预期值不匹配、似乎在该过程中发生了变化。

我向蓝牙堆栈传输按键数据的方法是否符合规格? 什么可能导致这种异常数据变化?

/*********************************************************************
 * @fn      Peripheral_AdvEventHandler
 *
 * @brief   The purpose of this function is to handle peripheral state
 *          events that rise from the GAP and were registered
 *          in @ref BLEAppUtil_registerEventHandler
 *
 * @param   event - message event.
 * @param   pMsgData - pointer to message data.
 *
 * @return  none
 */
static void Peripheral_AdvEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
{
//  if (pMsgData != NULL)
//  {
//    // Send the event to the upper layer
//    Peripheral_extEvtHandler(BLEAPPUTIL_GAP_ADV_TYPE, event, pMsgData);
//  }
    BLEAppUtil_AdvEventData_t *scanMsg = (BLEAppUtil_AdvEventData_t *)pMsgData;

    switch(event)
    {
        case BLEAPPUTIL_ADV_START_AFTER_ENABLE:
        {
            PHSCA_ESELOG_PRINTF("Adv status: Started - handle: %d", ((BLEAppUtil_AdvEventData_t *)pMsgData)->pBuf->advHandle);

            break;
        }

        case BLEAPPUTIL_ADV_END_AFTER_DISABLE:
        {
            PHSCA_ESELOG_PRINTF("Adv status: Ended - handle: %d", ((BLEAppUtil_AdvEventData_t *)pMsgData)->pBuf->advHandle);

            if(linkDB_NumActive() < linkDB_NumConns())
            {
                Peripheral_advStart(pMsgData);
            }

            break;
        }

        case BLEAPPUTIL_BUTTON_CLICK:
        {
            PHSCA_ESELOG_PRINTF("scanMsg->arg[0x%2x]\r\n", (*(scanMsg->arg))&0xFF);

            break;
        }

        default:
        {
            break;
        }
    }
}

此致!

普雷斯顿