This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LP-CC1352P7:是否可以使用灵活的开/关 BLE 接口?

Guru**** 2874300 points

Other Parts Discussed in Thread: BLE-STACK

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1562303/lp-cc1352p7-is-it-possible-to-have-a-flexible-on-off-ble-interface

器件型号:LP-CC1352P7
Thread 中讨论的其他器件:BLE-STACK

工具/软件:

您好!

我尝试向我的应用添加一项功能、需要按需打开和关闭 BLE 接口、以便从 手机应用等中央设备获取配置/调试数据。

基于 SimpleLink SDK、一旦 BLE 堆栈启动(这发生在 BIOS 启动之前)、一个无限循环将永远持续、并且一个名为 iCall 的调度器将用作事件回调机制。

因此、如果您启动 BLE 栈、 一旦完成 BLE 栈、就无法停止该栈、并且您无法 在运行时关闭此类接口。

我想知道是否可以在运行时使用开/关 BLE 接口 、如果可以、我如何做到这一点、

谢谢。