This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] 【常见问题解答】CC2745R10-Q1:未加载 CCS 20.3.0 安全调试管理器库

Guru**** 2928980 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1570016/faq-cc2745r10-q1-ccs-20-3-0-secure-debug-manager-libary-not-loaded

器件型号:CC2745R10-Q1


工具/软件:

问题:

尝试使用 CCS 20.3.0 刷写或调试 CC27XX 时、会报告以下错误:

Cortex_M33_0: Flash loader: CC23xx_CC27xx_FLASH_LIBRARY_VERSION 4.1.0.141
GEL: Error while executing OnPreTargetConnect(): Secure Debug Manager library not loaded!
         at GEL_LoadSecureDebugManager()
         at GEL_EvalOnTarget("CS_DAP_0", "GEL_LoadSecureDebugManager()") [cc23xx_xds.gel:81]
         at OnPreTargetConnect()
Error connecting to the target: (Error -2001 - (0:20:0)) Internal error: Invalid parameter passed to function. Restart the application. If error persists, please report the error. (Emulation package 20.3.0.3656) 
GEL: Error while executing OnRestart( 0 ): Connect failed
         at GEL_Connect() [cc23xx_connect_util.gel:41]
         at ConnectIfDisconnected() [cc23xx_xds.gel:101]
         at OnRestart(0)
AutoRun: Unable to run the target at this time
AutoRun: Target not run as breakpoint could not be set: Cannot enable while the target is disconnected
Target is not connected

这是因为此版本的 CCS 中包含的安全调试管理器 dll 缺少某些依赖项。

修复:

e2e.ti.com/.../SecureDebugManagerCC27_5F00_win.zip

下载 zip 文件、解压缩并替换中的内容   /ccs/ccs_base/DebugServer/bin/sdm

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的评分,丹尼尔!

    谢谢、

    Marie H