This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2340R5:需要一个用于创建 RTOS 任务的基本代码。

Guru**** 2927270 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1576198/cc2340r5-want-a-base-code-for-rtos-task-creation

器件型号:CC2340R5


工具/软件:

您好论坛、

我想作为单独的 RTOS 任务实施 TPMS 扫描、UART 通信。 另外、将来我可能想进行特定的 GATT 配置文件数据交换。 那么、您是否有任何用于任务创建的代码库?

此外、如果您可以为其建议步骤或文档、将会更好。

此致

Vaibhav

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您可以按照我们 用户指南中有关如何创建 FreeRTOS 任务的章节进行操作。

    示例代码如下所示

    #include <FreeRTOS.h>
    
    #include <task.h>
    
    #include <stdarg.h>
    
    
    #define TASK_PRIORITY 1
    
    #define TASK_STACK_SIZE 2048 /* bytes */
    
    
    TaskHandle_t taskHandle = NULL;
    
    
    /* Task function */
    
    void taskFunction(void* a0)
    
    {
    
        /* Local variables. Variables here go onto task stack!! */
    
    
        /* Run one-time code when task starts */
    
    
        while (1) /* Run loop forever (unless terminated) */
    
        {
    
            /*
    
             * Block on a signal or for a duration. Examples:
    
             *  ``xSemaphoreTake()``
    
             *  ``xQueueReceive``
    
             *  ``vTaskDelay()``
    
             *
    
             * "Process data"
    
             */
    
        }
    
    
        /* Tasks must not attempt to return from their implementing
    
        function or otherwise exit. If it is necessary for a task to
    
        exit then have the task call vTaskDelete( NULL ) to ensure
    
        its exit is clean. */
    
        vTaskDelete( NULL );
    
    }
    
    
    int main() {
    
    
        BaseType_t xReturned;
    
    
        /* Create the task, storing the handle. */
    
        xReturned = xTaskCreate(
    
                taskFxn,                                /* Function that implements the task. */
    
                "MY_NEW_TASK",                          /* Text name for the task. */
    
                TASK_STACK_SIZE / sizeof(uint32_t),     /* Stack size in words, not bytes. */
    
                ( void * ) 1,                           /* Parameter passed into the task. */
    
                TASK_PRIORITY,                          /* Priority at which the task is created. */
    
                &taskHandle );                                /* Used to pass out the created task's handle. */
    
    
        if(xReturned == errCOULD_NOT_ALLOCATE_REQUIRED_MEMORY)
    
        {
    
            /* Creation of FreeRTOS task failed */
    
            while(1);
    
        }
    
    
        /* Start the FreeRTOS scheduler */
    
                vTaskStartScheduler();
    
    
    }

    此致、
    Lea