This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2340R5-Q1:如何使用 HCI 命令输出载波频率

Guru**** 2905430 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1575999/cc2340r5-q1-how-to-output-the-carrier-frequency-using-hci-commands

器件型号:CC2340R5-Q1


工具/软件:

大家好、TI 团队。

我们想基于“Basic_ble"软件“软件使用 HCI 命令输出载波频率。

参考下面的链接、我们尝试执行 HCI_EXT_ModemTestTxCmd ()、但没有发生传输。

我们还粘贴了代码、因此如果有任何必要的程序或错误、请告知我们。

SDK 版本:9.11.

角色:外围设备

链接

void App_StackInitDoneHandler(gapDeviceInitDoneEvent_t *deviceInitDoneData)
{
    bStatus_t status = SUCCESS;

    // Menu
    Menu_start();

    // Print the device ID address
    MenuModule_printf(APP_MENU_DEVICE_ADDRESS, 0, "BLE ID Address: "
                      MENU_MODULE_COLOR_BOLD MENU_MODULE_COLOR_GREEN "%s" MENU_MODULE_COLOR_RESET,
                      BLEAppUtil_convertBdAddr2Str(deviceInitDoneData->devAddr));

    if ( appMainParams.addressMode > ADDRMODE_RANDOM)
    {
      // Print the RP address
        MenuModule_printf(APP_MENU_DEVICE_RP_ADDRESS, 0,
                     "BLE RP Address: "
                     MENU_MODULE_COLOR_BOLD MENU_MODULE_COLOR_GREEN "%s" MENU_MODULE_COLOR_RESET,
                     BLEAppUtil_convertBdAddr2Str(GAP_GetDevAddress(FALSE)));
    }

#if defined( HOST_CONFIG ) && ( HOST_CONFIG & ( PERIPHERAL_CFG | CENTRAL_CFG ) )
    status = DevInfo_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }
    status = SimpleGatt_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }
#endif

#if defined( HOST_CONFIG ) && ( HOST_CONFIG & ( PERIPHERAL_CFG | CENTRAL_CFG ))  &&  defined(OAD_CFG)
    status =  OAD_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }
#endif

#if defined( HOST_CONFIG ) && ( HOST_CONFIG & ( PERIPHERAL_CFG ) )
    // Any device that accepts the establishment of a link using
    // any of the connection establishment procedures referred to
    // as being in the Peripheral role.
    // A device operating in the Peripheral role will be in the
    // Peripheral role in the Link Layer Connection state.
    status = Peripheral_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }
#endif

#if defined( HOST_CONFIG ) && ( HOST_CONFIG & ( BROADCASTER_CFG ) )
    // A device operating in the Broadcaster role is a device that
    // sends advertising events or periodic advertising events
    status = Broadcaster_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }
#endif

#if defined( HOST_CONFIG ) && ( HOST_CONFIG & ( CENTRAL_CFG ) )
    // A device that supports the Central role initiates the establishment
    // of an active physical link. A device operating in the Central role will
    // be in the Central role in the Link Layer Connection state.
    // A device operating in the Central role is referred to as a Central.
    status = Central_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }
#endif

#if defined( HOST_CONFIG ) && ( HOST_CONFIG & ( OBSERVER_CFG ) )
    // A device operating in the Observer role is a device that
    // receives advertising events or periodic advertising events
    status = Observer_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }
#endif

#if defined( HOST_CONFIG ) && ( HOST_CONFIG & ( PERIPHERAL_CFG | CENTRAL_CFG ) )
    status = Connection_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }
    status = Pairing_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }
    status = Data_start();
    if(status != SUCCESS)
    {
        // TODO: Call Error Handler
    }

#if defined (BLE_V41_FEATURES) && (BLE_V41_FEATURES & L2CAP_COC_CFG)
    /* L2CAP COC Init */
    status = L2CAPCOC_start();
    if ( status != SUCCESS )
    {
    // TODO: Call Error Handler
    }
#endif //(BLE_V41_FEATURES) && (BLE_V41_FEATURES & L2CAP_COC_CFG)

    GPIO_setCallback(CONFIG_GPIO_DIO9, button_dio9_callback);       /* Add */
    GPIO_enableInt(CONFIG_GPIO_DIO9);                               /* Add */
#endif
}

void button_dio9_callback(uint_least8_t index)                      /* Add */
{

    BLEAppUtil_invokeFunctionNoData(hci_rf_cw_start);
}

extern uint8 peripheralAdvHandle_1;                                 /* Add */
void hci_rf_cw_start(char *dummy)                                   /* Add */
{

    GPIO_disableInt(CONFIG_GPIO_DIO9);
    GAP_TerminateLinkReq(Connection_getConnhandle(0), HCI_DISCONNECT_REMOTE_USER_TERM);
    GapAdv_disable(peripheralAdvHandle_1);
    HCI_EXT_SetTxPowerDbmCmd(0,1);
    HCI_EXT_ModemTestTxCmd(1,19);
}

/*********************************************************************
 * @fn      appMain
 *
 * @brief   Application main function
 *
 * @return  none
 */
void appMain(void)
{
    // Call the BLEAppUtil module init function
    BLEAppUtil_init(&criticalErrorHandler, &App_StackInitDoneHandler,
                    &appMainParams, &appMainPeriCentParams);
}

此致。