This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2745R10-Q1:未针对 Simplelink SDK 9.12 更新文档、用于提取绑定信息

Guru**** 2914580 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1584738/cc2745r10-q1-documents-not-updated-for-simplelink-sdk-9-12-for-extracting-bonding-information

器件型号: CC2745R10-Q1

你(们)好
  v 9.12 文档示例代码中提到的 API   gapBondMgrReadBondRec 替换为 GapBondMgr_readBondFromNV 构建块。
请使用正确的示例代码更新文档

 https://dev.ti.com/tirex/explore/content/simplelink_lowpower_f3_sdk_9_12_00_19/docs/ble5stack/ble_user_guide/html/ble-stack-5.x/gapbondmngr-cc23xx.html#extract-bonding-information  

 
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好:  

    这些文档将在接下来几天内的下一个版本中更新。 同时、我将为更新 GapBondMgr_readBondFromNV 函数提供以下代码片段。  

    // LOCAL VARIABLES
    
    // Array to save peer device's address
    static uint8_t peerDeviceAddr[B_ADDR_LEN];
    
    // enum to store peer device's address type
    static GAP_Peer_Addr_Types_t pPeerAddrType;
    
    void Peripheral_GAPConnEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
    {
        switch(event)
        {
            case BLEAPPUTIL_LINK_ESTABLISHED_EVENT:
            {
                gapEstLinkReqEvent_t *gapEstMsg = (gapEstLinkReqEvent_t *)pMsgData;
    
                if(gapEstMsg->connRole == BLEAPPUTIL_PERIPHERAL_ROLE)
                {
                  //...
                  //...
                  if (gapEstMsg->hdr.status == SUCCESS)
                  {
                      // Copy Peer's addr
                      memcpy(peerDeviceAddr, gapEstMsg->devAddr, B_ADDR_LEN);
    
                      // Copy Peer's addrType
                      pPeerAddrType = (GAP_Peer_Addr_Types_t)(gapEstMsg->devAddrType & MASK_ADDRTYPE_ID);
                  }
                //...
                //...
                }
            }
            break;
          //...
          //...

    // Parameters needed for storing bonding information.
    static gapBondNvRecord_t* pSavedBondRec;
    static uint8_t pIdentifier;
    static uint8_t readMode;
    
    uint8_t readStatus = FAILURE;
    readStatus = GapBondMgr_readBondFromNV(readMode,
                                           pIdentifier,
                                           pPeerAddrType,
                                           pSavedBondRec);
    if (readStatus == SUCCESS)
    {
        // If read success, then export the data
        // Here we will print it out for later use.
        // For the print, we added the following defines
        // Please consider your own example and modify as needed
        Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device Addr = [0x%02x, 0x%02x, 0x%02x, 0x%02x, 0x%02x, 0x%02x];", dispIndex,
                        pSavedBondRec->pBondRec->addr[0],
                        pSavedBondRec->pBondRec->addr[1],
                        pSavedBondRec->pBondRec->addr[2],
                        pSavedBondRec->pBondRec->addr[3],
                        pSavedBondRec->pBondRec->addr[4],
                        pSavedBondRec->pBondRec->addr[5]); dispIndex++;
    
        Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device AddrType = 0x%02x; stateFlag = 0x%02x;", dispIndex, pSavedBondRec->pBondRec->addrType, pSavedBondRec->pBondRec->stateFlags); dispIndex++;
        Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device AddrType = 0x%02x; stateFlag = 0x%02x;", dispIndex, pSavedBondRec->pBondRec->addrType, pSavedBondRec->pBondRec->stateFlags); dispIndex++;
        Display_printf(dispHandle, dispIndex, 0, "#%5d    Local Device eDiv = 0x%02x; keySize = 0x%02x;", dispIndex, pSavedBondRec->pLocalLtk->div, pSavedBondRec->pLocalLtk->keySize); dispIndex++;
        Display_printf(dispHandle, dispIndex, 0, "#%5d    Peer Device SignCount = 0x%08x;", dispIndex, pSavedBondRec->pSignCount); dispIndex++;
    }
    break;

    谢谢、  

    Isaac