This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2540:在没有加密狗的情况下连接(使用笔记本电脑 BLE 芯片组)

Guru**** 2943350 points

Other Parts Discussed in Thread: CC2540, ADS1293

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1087603/cc2540-connect-without-dongle-using-laptop-ble-chipset

部件号:CC2540
“线程: ADS1293”中讨论的其它部件

请告诉我需要做些什么来从我的笔记本电脑上删除加密狗 CC2540,而是依靠我的笔记本电脑上的双人电脑!

我在您的 ads1293参考设计视频中看到苹果平板电脑可能会出现这种情况。

谢谢你 e2e。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

    如果您的 PC 有 BLE 芯片,那么您应该能够扫描蓝牙设备并连接到允许连接的任何设备。 但是,您的操作系统可能会限制您在使用 BLE 连接时可以执行的操作,甚至限制您可以与哪些设备建立连接。 有关详细信息,请参阅您首选操作系统中提供的文档。

    以下 BLE 示例依赖于连接到 PC,可能会有所帮助:

    HID over GATT Profile (HOGP) BLE 应用说明

    HOGP-BLE-HID 示例

    此致,

    1月