This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2642R:使用 BLE SoC 为外设供电

Guru**** 2589300 points
Other Parts Discussed in Thread: TMP117, LPSTK-CC1352R, CC2650STK

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1024325/cc2642r-powering-peripheral-with-a-ble-soc

器件型号:CC2642R
主题中讨论的其他器件:TMP117LPSTK-CC1352RCC2650STK

您好!

我正在设计一个具有 BLE SoC 和温度传感器的系统- TMP117。  我正在尝试寻找功耗最低、成本最低的解决方案。  TMP117可在1.7V 至5.5V 电压 μA 内运行、电流消耗通常为3.5 μ A。  BLE SoC 由 3V 纽扣电池供电。  根据我的理解、我们产品系列中的所有 BLE SoC 都能够为 TMP117供电。    

最初、我让 BLE SoC 控制纽扣电池和 TMP117之间的负载开关(左图)。  但是、消除负载开关会节省大量功耗和成本。   无负载开关的理想解决方案是否起作用?

一  

感谢专家的确认

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Alexander、

    是的、右侧的配置应该可以正常工作。  您还可以参阅 CC2650STK 或 LPSTK-CC1352R、了解有关设计具有传感器的 BLE SoC (以及纽扣电池供电)的其他示例。

    谢谢、

    Alexis