This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2564:CC2564B BLE @Δ"RF-PHY 4.2@TP/RCV-LE/BV-03-C[C/I 和1ms&quot 下的接收器选择性能;

Guru**** 2587285 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/760485/cc2564-cc2564b-ble-testing-rf-phy-4-2-tp-rcv-le-ca-bv-03-c-c-i-and-receiver-selectivity-performance-at-1ms-s

器件型号:CC2564

您好、e2e、

我们的客户正在其项目中使用 CC2564B、现在正在以 1ms/s 的速度执行 BLE 部件测试@"RF-PHY 4.2@TP/RCV-LE/BV-03-C[C/I 和接收器选择性能"。

 测试过程中有一个参数 Image Frequency (图像频率)配置为-1MHz、他们发现2426MHz 和2476MHz 无法通过测试。

你对此有什么建议吗?

图像频率值-1MHz 是否正确? 我们在 CC2564B 数据表中找到它、如下所示。

谢谢。

Leon