This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-CC2650:UART 转 BLE 桥接器问题

Guru**** 2553450 points
Other Parts Discussed in Thread: CC2650

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/583019/launchxl-cc2650-uart-to-ble-bridge-question

器件型号:LAUNCHXL-CC2650
Thread 中讨论的其他器件:CC2650

您好!

我让 UART 转 BLE 桥工作(SPP_BLE_CLIENT 和 SPP_BLE_SERVER)、并且我可以使用计算机上的 Putty 通过串行接口在2个 cc2650 LaunchPad 之间发送接收数据。 我的问题是如何获取其中一个 LaunchPad 接收到的要通过 RX 引脚(SO 引脚 IOID_2)发送的数据? 因此、当 LaunchPad 板通过无线方式(通过 BLE)接收数据时、它不是通过板上的 RX 引脚发送到我的计算机上的终端窗口。

谢谢