请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:CC2541 您好!
我想知道如何更改 BLE 1.4.1上 CC2541 PA 控制引脚的 IO 配置。
PA 与 CC2541集成的典型配置位于端口 P1_2 (Tx)和 P1_3 (Rx)上、但在其中一个设计中、它分别连接到 P1_1和 P1_0、因此需要重新配置 IO。
等待论坛的快速响应。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.