This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2650STK:CC2650 STK PDM 驱动程序问题

Guru**** 2576195 points
Other Parts Discussed in Thread: CC2640R2F, BLE-STACK

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/588513/cc2650stk-cc2650-stk-pdm-driver-issue

器件型号:CC2650STK
Thread 中讨论的其他器件:CC2640R2FBLE-STACK

大家好、

我正在处理以下案例:

我使用 Sensortag CC2650 音频示例将音频从 Sensortag 流式传输 到 Raspberry Pi。 有 了 Sensortag、我将使用 BLE-Stack 2.2.1 和 TI-TROS  2.20.01.08。  

我能够启动音频示例并通过两种不同的方式获取音频:1)通过 BLE 发送音频2)通过 UART 接口发送音频。 但是、在任何情况下、我都会以非常独特的模式丢失音频帧。也就是说 、在 HAR_AUDIO_MAX_ALLOC_BUF 设置为10 (默认值)的情况下、我始终可以接收前10帧而不会丢失任何数据。 如果我将 HAR_AUDIO_MAX_ALLOC_BUF 更改为其他值(使用5、15、20、25和30进行测试)、则趋势仍然存在。

为了更清楚地说明、我要附加一个用于音频解码的日志文件片段、我使用音频解码 Python 脚本的修改版本获得了该文件(请参阅 此处 的文件"Audio 帧串行打印.py")。 在示例中、我使用 了 HAR_AUDIO_MAX_ALLOC_BUF 设置为10并录制了音频10秒( "sensortag_audio.c"中的恒定 HAR_STREALL_TIMER 设置为10000)。

1
2.
3.
4.
5.
6.
7.
8.
9.
10.
11.
12.
13.
14.
15.
16.
17.
18
19.
20.
21.
22.
23
24
25
26
27.
28.
29.
30
31.
32
33.
34
35.
36.
37.
38.
39.
40
41.
42.
43.
44.
45.
46.
47.
48
49
50
51.
52.
53.
54
55
56.
57.
58.
59.
60
61.
62.
63.
64
65
66
67
68
69
70
71.
72.
73.
74.
75
76.
77
78
79
80
81.
82.
83.
84
85.
86
87
88
89
90
91.
92
93
94
95
96
97
98
99
100
101.
102.
103.
104.
105.
106.
107.
108.
109.
110
111.
112
113
114
115
116
117
118
119
Frame sequence number: 1
HDR_1 local: 0, HDR_1 received: 0
HDR_2 local: 0, HDR_2 received: 0
Frame sequence number: 2
HDR_1 local: 18, HDR_1 received: 18
HDR_2 local: -136, HDR_2 received: -136
Frame sequence number: 3
HDR_1 local: 20, HDR_1 received: 20
HDR_2 local: 2, HDR_2 received: 2
Frame sequence number: 4
HDR_1 local: 26, HDR_1 received: 26
HDR_2 local: -129, HDR_2 received: -129
Frame sequence number: 5
HDR_1 local: 14, HDR_1 received: 14
HDR_2 local: -33, HDR_2 received: -33
Frame sequence number: 6
HDR_1 local: 14, HDR_1 received: 14
HDR_2 local: -139, HDR_2 received: -139
Frame sequence number: 7
HDR_1 local: 16, HDR_1 received: 16
HDR_2 local: -108, HDR_2 received: -108
Frame sequence number: 8
HDR_1 local: 25, HDR_1 received: 25
HDR_2 local: -148, HDR_2 received: -148
Frame sequence number: 9
HDR_1 local: 22, HDR_1 received: 22
HDR_2 local: -75, HDR_2 received: -75
Frame sequence number: 10
HDR_1 local: 39, HDR_1 received: 39
HDR_2 local: 295, HDR_2 received: 295
Frame sequence number: 11
HDR_1 local: 38, HDR_1 received: 38
HDR_2 local: -391, HDR_2 received: -391
Frame sequence number: 12
HDR_1 local: 29, HDR_1 received: 29
HDR_2 local: -28, HDR_2 received: -28
Frame sequence number: 13
HDR_1 local: 23, HDR_1 received: 23
HDR_2 local: -153, HDR_2 received: -153
Frame sequence number: 14
HDR_1 local: 23, HDR_1 received: 23
HDR_2 local: -7, HDR_2 received: -7
Frame sequence number: 15
HDR_1 local: 19, HDR_1 received: 19
HDR_2 local: -61, HDR_2 received: -61
Frame sequence number: 16
HDR_1 local: 14, HDR_1 received: 14
HDR_2 local: -62, HDR_2 received: -62
Frame sequence number: 17
HDR_1 local: 34, HDR_1 received: 34
HDR_2 local: -304, HDR_2 received: -304
Frame sequence number: 18
HDR_1 local: 29, HDR_1 received: 29
HDR_2 local: 127, HDR_2 received: 127
Frame sequence number: 19
HDR_1 local: 26, HDR_1 received: 26
HDR_2 local: 126, HDR_2 received: 126
Frame sequence number: 20
HDR_1 local: 31, HDR_1 received: 31
HDR_2 local: -114, HDR_2 received: -114
Frame sequence number: 22
HDR_1 local: 35, HDR_1 received: 35
HDR_2 local: 146, HDR_2 received: 146
######################### MISSED #########################
1
##########################################################
Frame sequence number: 23
HDR_1 local: 38, HDR_1 received: 38
HDR_2 local: 119, HDR_2 received: 119
Frame sequence number: 24
HDR_1 local: 31, HDR_1 received: 31
HDR_2 local: -187, HDR_2 received: -187
Frame sequence number: 25
HDR_1 local: 23, HDR_1 received: 23
HDR_2 local: -73, HDR_2 received: -73
Frame sequence number: 27
HDR_1 local: 28, HDR_1 received: 28
HDR_2 local: -166, HDR_2 received: -166
######################### MISSED #########################
1
##########################################################
Frame sequence number: 28
HDR_1 local: 22, HDR_1 received: 22
HDR_2 local: 11, HDR_2 received: 11
Frame sequence number: 29
HDR_1 local: 25, HDR_1 received: 25
HDR_2 local: 37, HDR_2 received: 37
Frame sequence number: 30
HDR_1 local: 36, HDR_1 received: 36
HDR_2 local: 294, HDR_2 received: 294
Frame sequence number: 0
HDR_1 local: 20, HDR_1 received: 20
HDR_2 local: -14, HDR_2 received: -14
######################### MISSED #########################
1
##########################################################
Frame sequence number: 1
HDR_1 local: 31, HDR_1 received: 31
HDR_2 local: -292, HDR_2 received: -292
Frame sequence number: 2
HDR_1 local: 39, HDR_1 received: 39
HDR_2 local: -415, HDR_2 received: -415
Frame sequence number: 3
HDR_1 local: 25, HDR_1 received: 25
HDR_2 local: 142, HDR_2 received: 142
Frame sequence number: 5
HDR_1 local: 27, HDR_1 received: 27
HDR_2 local: 197, HDR_2 received: 197
######################### MISSED #########################
1
##########################################################
...
saving file
...DONE...
Frames lost: 168
Frames received: 658

使用此示例、我将解释我遇到的怪异情况。 在第二个块的帧 (例如接下来的10个帧)中、通常会丢失一个帧、通常在第三个块的末尾或在第三个块的开头、如本例所示。 例如、从1到10的帧被成功接收、这样从11到20的帧、而第三个块的第一个帧丢失(序列编号21)。 第一个帧的丢失有所不同、但从我的实验来看、它通常"接近"第二个块的末尾或第三个块的开头。 同样、块大小取决于 HAR_AUDIO_MAX_ALLOC_BUF 值、其他值的趋势完全相同。  

在第一个丢失帧后、新的趋势开始、第一个丢失帧后的每五个帧丢失。 也就是说、在示例中、第一个丢失帧的序列号为21、然后我们正确接收4个帧(22-25)、然后再次丢失帧26。 这种趋势在整个音频录制期间持续,我没有观察到对可调参数的任何依赖(例如 Har_AUDIO_MAX_ALLOC_BUF 或 HAR_STREAM_LIMIT_TIME )。 更糟糕的是、丢失一个帧是最常见的、但不是唯一的选择。 在我的许多试验中,我一直观察到连续两帧丢失的情况。 虽然这种情况比丢失一帧的频率要低得多、但仍然非常持久。  

我开始调试这个问题、结果发现这个问题导致"sensortag_audio.c"中的以下代码行:  

1
tmpSeqNum = (((PDMCC26XX_pcmBuffer *)pAudioFrame)->metaData).seqNum;

这意味着丢失的序列号是由 PDM 驱动程序而不是 BLE-STACK 或任何其他组件引起的。 为了增加可用存储器的容量、我禁用了所有其他传感器以及其他服务、例如电池、OAD、I/O、电池和工厂复位。 问题仍然存在。

在我看来、PDM 驱动程序中有一个错误、这会导致一些内存问题(例如溢出)、从而导致帧丢失。 那么、TI 专家面临的问题是如何解决这个问题? 这可能是编解码器的问题、因为帧丢失与 4:1压缩率具有非常明显的相关性(在许多试验中、我观察到帧丢失约为25%及更高)?

有人能帮我解决这个问题吗?

谢谢你。

考乌什

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Kaustuh、您好!

    感谢您的深入介绍和格式正确的帖子。 通过 BLE 对语音进行采样和流式传输有许多相关因素。

    在开始之前、我想向您指出一个用于语音/PDM 驱动程序信息的优秀资源。 尽管它是为 CC2640R2F 编写的,但所有概念都适用于两个 CC26xx 器件:

    调试语音流问题是一个包含3个步骤的过程

    1.确保在流媒体上正确采样/处理语音(即 sensortag_audio)。 在没有 BLE 链路的情况下应该/可以执行这些测试。 理想情况下、在这些步骤期间、BLE-STACK 将处于空闲状态。 我会从上到下查看下面的项目符号。

    • 维修 PDM 驱动程序的应用程序是否足够频繁? 用户应用程序必须每2ms 对 PDM 驱动程序进行一次采样是一项硬性要求、否则、PDM 驱动程序将丢弃帧、以便为新帧腾出空间。 您可以通过在应用程序读取 PDM 帧时切换 GPIO 并使用逻辑分析仪来测量时间来配置此配置文件。 很可能是因为某种原因导致 PDM 处理延迟、从而导致帧丢失。
    • 如果您的应用程序需要2ms 以上的时间来处理帧、您可以增加 PDM 驱动程序端分配的缓冲区数量、但代价是延迟和 RAM、要这样做的定义是 minimum_pdm_buffer_queue_depth
    • 硬件设置是否正确、BCLK 和 AD0是否正确。 BCLK 是正确的频率、没有毛刺脉冲。 当您看到丢失的帧时、请检查 I2S 错误。
    • 确保 python 脚本运行正确且足够快。 为此、您可以将音频直接从 sensortag 转储到 python 脚本、而无需 BLE。  我还将确保使用此处的最新版本的脚本:  

    2、假设上述所有测试均已完成、您就可以将 BLE 添加到公式中了。  

    • 检查射频条件、由于 BLE 在控制器级别处理数据包重试的方式(通过 Rack/NACK 系统实现可靠)、边缘射频条件可能会延迟 BLE 数据包的传输、并导致接收端无法满足实时吞吐量要求
    • 请注意   、BLE 所需的吞吐量为 136.67kbps
    • 这相当于每秒417次通知。 如果您的对等设备不允许这种吞吐量、您可能无法正确地流式传输数据。 我建议使用   连接间隔为10ms 的来接收 BLE 语音。

    接收端必须解包 BLE 数据包并正确发送到 python 脚本。 这通过使用 simple_central 音频接收器的 STRE_TO_PC 选项进行演示。