This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2564:CC2564B 是否可以像经典一样被发现/可连接、以及发送 BLE 广播?

Guru**** 2583395 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/710909/cc2564-is-it-possible-for-the-cc2564b-to-be-discoverable-connectable-as-classic-as-well-as-send-out-ble-advertisements

器件型号:CC2564

为了清楚地了解我的预期用例、在连接发生后、CC2564B 肯定会致力于单种通信(即仅经典通信或仅 BLE 通信)。  它位于我感兴趣的连接之前

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好!

    是的、CC2564B 可以进行广播、同时进行查询扫描和页面扫描(可发现/可连接)。

    此外、在连接发生后、CC2564B 还可以同时连接到 BLE 和 BT Classic -但是、您需要确保连接参数能够使这两个连接共存。

    BR、
    陈洛威