This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2540:如何在 BLE 连接中禁用加密

Guru**** 2540720 points
Other Parts Discussed in Thread: CC2540

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/702225/cc2540-how-disable-encryption-in-ble-connetction

器件型号:CC2540

大家好!

我是 BLE 的新用户、我有一个示例、其中 CC2540在 BLE 连接中发挥核心作用、我希望使用监听器来查看 BLE 数据包、但连接已加密。 我想知道如何在 CC2540端禁用加密。 在下图中、您可以看到主器件发送的 LL_encryption_SEQ、在我的情况下为 CC2540。

谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Alireza、

    尝试禁用配对:

     //设置 GAP 绑定管理器

     {

      uint32密钥= 0;//密钥"000000"

      uint8配对模式= GAPBOND_Pairing_mode_no_pairing;

    (笑声)