This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] Linux/CC2564C:如果启用了 BLE 并且广播信标数据包时、BT 经典(BR/EDR)是否处于可发现模式?

Guru**** 2763595 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/723653/linux-cc2564c-is-the-bt-classic-br-edr-in-discoverable-mode-if-ble-is-enabled-and-is-advertising-beacon-packet

器件型号:CC2564C

工具/软件:Linux

您好!

如果启用了 BLE 并且正在广播信标数据包、则 BT 经典(BR/EDR)是否处于可发现模式? 或者、当经典处于可发现状态或启用 BLE 时、此 BT 芯片是否可发现(例如通过智能手机)?

如果没有,是否有激活 BLE 的方法,同时也无法发现 BT 经典?

谢谢。