This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2640R2F:当 CC2640的广播间隔设置为大于7.5s 时、BLE 扫描仪应用程序无法连接到 CC2640

Guru**** 2390785 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1207150/cc2640r2f-when-advertising-interval-of-cc2640-is-set-to-more-than-7-5-secs-ble-scanner-app-is-not-able-to-connect-to-cc2640

器件型号:CC2640R2F

我正在使用 BLE Zero 项目、并尝试在睡眠模式下增加广播间隔。 但当我尝试将时间间隔增加到7.5秒以上时、连接始终会失败。 我将使用" GapAdv_setParam"更改间隔值。 我还需要修改什么内容吗、或者我缺少什么内容吗? 如果我不熟悉 BLE、请提供帮助。

static void ProjectZero_processGapMessage(gapEventHdr_t *pMsg)
{
    switch(pMsg->opcode)
    {
    case GAP_DEVICE_INIT_DONE_EVENT:
    {
        bStatus_t status = FAILURE;

        gapDeviceInitDoneEvent_t *pPkt = (gapDeviceInitDoneEvent_t *)pMsg;

        if(pPkt->hdr.status == SUCCESS)
        {
            // Store the system ID
            uint8_t systemId[DEVINFO_SYSTEM_ID_LEN];

            // use 6 bytes of device address for 8 bytes of system ID value
            systemId[0] = pPkt->devAddr[0];
            systemId[1] = pPkt->devAddr[1];
            systemId[2] = pPkt->devAddr[2];

            // set middle bytes to zero
            systemId[4] = 0x00;
            systemId[3] = 0x00;

            // shift three bytes up
            systemId[7] = pPkt->devAddr[5];
            systemId[6] = pPkt->devAddr[4];
            systemId[5] = pPkt->devAddr[3];

            // Set Device Info Service Parameter
            DevInfo_SetParameter(DEVINFO_SYSTEM_ID, DEVINFO_SYSTEM_ID_LEN,
                                 systemId);

            // Display device address
            // Need static so string persists until printed in idle thread.
            static uint8_t addrStr[3 * B_ADDR_LEN + 1];
            util_arrtohex(pPkt->devAddr, B_ADDR_LEN, addrStr, sizeof addrStr,
                          UTIL_ARRTOHEX_REVERSE);
            Log_info1("GAP is started. Our address: " \
                      ANSI_COLOR(FG_GREEN) "%s" ANSI_COLOR(ATTR_RESET),
                      (uintptr_t)addrStr);

            // Setup and start Advertising
            // For more information, see the GAP section in the User's Guide:
            // software-dl.ti.com/.../

            // Temporary memory for advertising parameters for set #1. These will be copied
            // by the GapAdv module
            GapAdv_params_t advParamLegacy = GAPADV_PARAMS_LEGACY_SCANN_CONN;

            // Create Advertisement set #1 and assign handle
            status = GapAdv_create(&ProjectZero_advCallback, &advParamLegacy,
                                   &advHandleLegacy);
            APP_ASSERT(status == SUCCESS);

            Log_info1("Name in advertData array: " \
                      ANSI_COLOR(FG_YELLOW) "%s" ANSI_COLOR(ATTR_RESET),
                      (uintptr_t)util_getLocalNameStr(advertData,
                                                      sizeof(advertData)));

            // Load advertising data for set #1 that is statically allocated by the app
            status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_ADV,
                                         sizeof(advertData), advertData);
            APP_ASSERT(status == SUCCESS);

            // Load scan response data for set #1 that is statically allocated by the app
            status =
                GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_SCAN_RSP,
                                    sizeof(scanRspData),
                                    scanRspData);
            APP_ASSERT(status == SUCCESS);

            // Set event mask for set #1
            status = GapAdv_setEventMask(advHandleLegacy,
                                         GAP_ADV_EVT_MASK_START_AFTER_ENABLE |
                                         GAP_ADV_EVT_MASK_END_AFTER_DISABLE |
                                         GAP_ADV_EVT_MASK_SET_TERMINATED);
            //newAdvInt*625= time interval in us
            //changed by Ankit
            uint32_t newAdvInt = 11200;//8000; //3200;
                       GapAdv_setParam(advHandleLegacy, GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN, &newAdvInt);
                       GapAdv_setParam(advHandleLegacy, GAP_ADV_PARAM_TX_POWER,20);
                       newAdvInt = 11200;
                       GapAdv_setParam(advHandleLegacy, GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX, &newAdvInt);
            // Enable legacy advertising for set #1
            status =
                GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX, 0);
           // advhandle=advHandleLegacy;
                  //  GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_DURATION, 2000);
            APP_ASSERT(status == SUCCESS);
        }

        break;
    }

    case GAP_LINK_ESTABLISHED_EVENT:
    {
        gapEstLinkReqEvent_t *pPkt = (gapEstLinkReqEvent_t *)pMsg;

        // Display the amount of current connections
        Log_info2("Link establish event, status 0x%02x. Num Conns: %d",
                  pPkt->hdr.status,
                  linkDB_NumActive());

        if(pPkt->hdr.status == SUCCESS)
        {
            // Add connection to list
            ProjectZero_addConn(pPkt->connectionHandle);

            // Display the address of this connection
            static uint8_t addrStr[3 * B_ADDR_LEN + 1];
            util_arrtohex(pPkt->devAddr, B_ADDR_LEN, addrStr, sizeof addrStr,
                          UTIL_ARRTOHEX_REVERSE);
            Log_info1("Connected. Peer address: " \
                        ANSI_COLOR(FG_GREEN)"%s"ANSI_COLOR(ATTR_RESET),
                      (uintptr_t)addrStr);
        }

        if(linkDB_NumActive() < MAX_NUM_BLE_CONNS)
        {
            Log_info1("Continue to Advertise, %d possible connection remain", MAX_NUM_BLE_CONNS - linkDB_NumActive());
            // Start advertising since there is room for more connections
            GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX, 0);
        }
        else
        {
            Log_info1("Max Number of Connection reach: %d, Adv. will not be enable again", linkDB_NumActive());
        }
    }
    break;

    case GAP_LINK_TERMINATED_EVENT:
    {
        gapTerminateLinkEvent_t *pPkt = (gapTerminateLinkEvent_t *)pMsg;

        // Display the amount of current connections
        Log_info0("Device Disconnected!");
        Log_info1("Num Conns: %d", linkDB_NumActive());

        // Remove the connection from the list and disable RSSI if needed
        ProjectZero_removeConn(pPkt->connectionHandle);

        // GapAdv_enable will return success only if the maximum number of connections 
		// has been reached, and adv was not re-enable in GAP_LINK_ESTABLISHED_EVENT
		// switch case.
        // If less connection were in used, Advertisement will have been restart in 
		// the GAP_LINK_ESTABLISHED_EVENT switch case and calling GapAdv_enable will 
		// just return an error.
        if ( GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX, 0) == SUCCESS)
        {
            Log_info1("Restart Advertising, %d possible connection remain", MAX_NUM_BLE_CONNS - linkDB_NumActive());
        }
    }
    break;

    case GAP_UPDATE_LINK_PARAM_REQ_EVENT:
        ProjectZero_handleUpdateLinkParamReq(
            (gapUpdateLinkParamReqEvent_t *)pMsg);
        break;

    case GAP_LINK_PARAM_UPDATE_EVENT:
        ProjectZero_handleUpdateLinkEvent((gapLinkUpdateEvent_t *)pMsg);
        break;

    case GAP_PAIRING_REQ_EVENT:
        // Disable advertising so that the peer device can be added to
        // the resolving list
        GapAdv_disable(advHandleLegacy);
        break;

    default:
        break;
    }
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Ankit、您好!

    感谢您与我们联系、

    您可以查看射频输出的实际情况、请查看 SDK 中 BLE5Stack 用户指南的调试部分。

    关于您的问题,这是您在项目上唯一更改的内容吗? 此项目的扫描参数(扫描持续时间、扫描间隔和扫描窗口)是什么?

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我添加了用于从传感器获取数据的 SPI 任务、但关于 BLE 器件、是的、这是我唯一更改的东西。 对于扫描我正在使用 BLE 扫描仪应用程序,所以不知道它的扫描参数是什么。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    它是否适用于短于7.5秒的广告间隔?

    您有一些蓝牙监听器跟踪吗? 对于这个问题、它将有很大帮助。

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、它在间隔短于7.5s 的情况下运行良好。 但我认为您是对的、我应该尝试蓝牙监听器或其他 BLE 应用、以查看问题是否仍然存在。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    理想情况下,我可以保持的最大间隔应该是多少,以便它能够顺利地连接到应用程序而不会失败?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    理论上、广播间隔值的范围从20毫秒一直到10.24秒、增量很小、为625微秒。

    当您有迹线时、请告诉我。

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    连接问题已解决、这不是设备问题、而是 BLE 扫描仪应用的问题。 当尝试 NRF BLE 扫描仪应用程序时,它能够成功地检测和连接它。