This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2652R:CC2652R 和 CC2640R2F 之间的连接始终快速终止

Guru**** 2618835 points

Other Parts Discussed in Thread: CC2652R, CC2640R2F

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1203832/cc2652r-connection-between-cc2652r-and-cc2640r2f-always-terminates-quickly

器件型号:CC2652R
主题中讨论的其他器件: CC2640CC2640R2F

CC2652R 由 BTOOL 使用 SDK 6.20进行处理

CC2640R2F SDK 5.30 e2e.ti.com/.../5824.CC2640.rar

 和 BTOOL 中的部分日志。 断开连接还有其他一些原因、例如0x3E。 我尝试关闭其他 BLE 设备、但失败了。  

[1] : <Tx> - 06:46:12.865
-Type           : 0x01 (Command)
-OpCode         : 0xFE62 (GapInit_connect)
-Data Length    : 0x0A (10) byte(s)
 PeerAddrType   : 0x00 (0) (PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID)
 PeerAddr       : 60:77:71:C7:9F:A2
 InitiatingPhy  : 0x01 (1) (
                  INIT_PHY_1M)
 Timeout        : 0x0000 (0)
Dump(Tx):
0000:01 62 FE 0A 00 A2 9F C7 71 77 60 01 00 00       .b......qw`...
--------------------------------------------------------------------
[2] : <Rx> - 06:46:12.879
-Type           : 0x04 (Event)
-EventCode      : 0x00FF (HCI_LE_ExtEvent)
-Data Length    : 0x06 (6) bytes(s)
 Event          : 0x067F (1663) (GAP_HCI_ExtentionCommandStatus)
 Status         : 0x11 (17) (bleAlreadyInRequestedMode)
 OpCode         : 0xFE62 (GapInit_connect)
 DataLength     : 0x00 (0)
Dump(Rx):
0000:04 FF 06 7F 06 11 62 FE 00                      ......b..
--------------------------------------------------------------------
[3] : <Warning> - 06:46:42.858
GAP Link Establish Request Timeout
--------------------------------------------------------------------
[4] : <Tx> - 06:47:24.059
-Type           : 0x01 (Command)
-OpCode         : 0xFE62 (GapInit_connect)
-Data Length    : 0x0A (10) byte(s)
 PeerAddrType   : 0x00 (0) (PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID)
 PeerAddr       : 60:77:71:C7:9F:A2
 InitiatingPhy  : 0x01 (1) (
                  INIT_PHY_1M)
 Timeout        : 0x0000 (0)
Dump(Tx):
0000:01 62 FE 0A 00 A2 9F C7 71 77 60 01 00 00       .b......qw`...
--------------------------------------------------------------------
[5] : <Rx> - 06:47:24.074
-Type           : 0x04 (Event)
-EventCode      : 0x00FF (HCI_LE_ExtEvent)
-Data Length    : 0x06 (6) bytes(s)
 Event          : 0x067F (1663) (GAP_HCI_ExtentionCommandStatus)
 Status         : 0x11 (17) (bleAlreadyInRequestedMode)
 OpCode         : 0xFE62 (GapInit_connect)
 DataLength     : 0x00 (0)
Dump(Rx):
0000:04 FF 06 7F 06 11 62 FE 00                      ......b..
--------------------------------------------------------------------
[6] : <Warning> - 06:47:54.079
GAP Link Establish Request Timeout
--------------------------------------------------------------------
[7] : <Rx> - 06:48:08.667
-Type           : 0x04 (Event)
-EventCode      : 0x00FF (HCI_LE_ExtEvent)
-Data Length    : 0x14 (20) bytes(s)
 Event          : 0x0605 (1541) (GAP_EstablishLink)
 Status         : 0x00 (0) (SUCCESS)
 DevAddrType    : 0x00 (0) (ADDRTYPE_PUBLIC)
 DevAddr        : 60:77:71:C7:9F:A2
 ConnHandle     : 0x0000 (0)
 ConnRole       : 0x08 (8) (
                  Central)
 ConnInterval   : 0x0050 (80)
 ConnLatency    : 0x0000 (0)
 ConnTimeout    : 0x07D0 (2000)
 ClockAccuracy  : 0x00 (0)
Dump(Rx):
0000:04 FF 14 05 06 00 00 A2 9F C7 71 77 60 00 00 08 ..........qw`...
0010:50 00 00 00 D0 07 00                            P......
--------------------------------------------------------------------
[8] : <Tx> - 06:48:08.669
-Type           : 0x01 (Command)
-OpCode         : 0x2022 (HCI_LE_SetDataLength)
-Data Length    : 0x06 (6) byte(s)
 Handle         : 0x0000 (0)
 TxOctets       : 0x00FB (251)
 TxTime         : 0x0848 (2120)
Dump(Tx):
0000:01 22 20 06 00 00 FB 00 48 08                   ." .....H.
--------------------------------------------------------------------
[9] : <Info> - 06:48:08.742
Device Connected
Handle = 0x0000
Addr Type = 0x00 (ADDRTYPE_PUBLIC)
BDAddr = 60:77:71:C7:9F:A2
--------------------------------------------------------------------
[10] : <Rx> - 06:48:08.733
-Type           : 0x04 (Event)
-EventCode      : 0x000E (HCI_CommandCompleteEvent)
-Data Length    : 0x06 (6) bytes(s)
 Packets        : 0x01 (1)
 OpCode         : 0x2022 (HCI_LE_SetDataLength)
 Status         : 0x00 (0) (SUCCESS)
 Handle         : 0x0000 (0)
Dump(Rx):
0000:04 0E 06 01 22 20 00 00 00                      ...." ...
--------------------------------------------------------------------
[11] : <Info> - 06:48:09.254
Device Disconnected
Handle = 0x0000
Addr Type = 0x00 (ADDRTYPE_PUBLIC)
BDAddr = 60:77:71:C7:9F:A2
--------------------------------------------------------------------
[12] : <Rx> - 06:48:09.252
-Type           : 0x04 (Event)
-EventCode      : 0x00FF (HCI_LE_ExtEvent)
-Data Length    : 0x06 (6) bytes(s)
 Event          : 0x0606 (1542) (GAP_TerminateLink)
 Status         : 0x00 (0) (SUCCESS)
 ConnHandle     : 0x0000 (0)
 Reason         : 0x3E (62) (FAILED_TO_ESTABLISH)
Dump(Rx):
0000:04 FF 06 06 06 00 00 00 3E                      ........>
--------------------------------------------------------------------
[13] : <Tx> - 06:48:16.341
-Type           : 0x01 (Command)
-OpCode         : 0xFE62 (GapInit_connect)
-Data Length    : 0x0A (10) byte(s)
 PeerAddrType   : 0x00 (0) (PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID)
 PeerAddr       : 60:77:71:C7:9F:A2
 InitiatingPhy  : 0x01 (1) (
                  INIT_PHY_1M)
 Timeout        : 0x0000 (0)
Dump(Tx):
0000:01 62 FE 0A 00 A2 9F C7 71 77 60 01 00 00       .b......qw`...
--------------------------------------------------------------------
[14] : <Rx> - 06:48:16.361
-Type           : 0x04 (Event)
-EventCode      : 0x00FF (HCI_LE_ExtEvent)
-Data Length    : 0x06 (6) bytes(s)
 Event          : 0x067F (1663) (GAP_HCI_ExtentionCommandStatus)
 Status         : 0x00 (0) (SUCCESS)
 OpCode         : 0xFE62 (GapInit_connect)
 DataLength     : 0x00 (0)
Dump(Rx):
0000:04 FF 06 7F 06 00 62 FE 00                      ......b..
--------------------------------------------------------------------
[15] : <Rx> - 06:48:16.456
-Type           : 0x04 (Event)
-EventCode      : 0x00FF (HCI_LE_ExtEvent)
-Data Length    : 0x14 (20) bytes(s)
 Event          : 0x0605 (1541) (GAP_EstablishLink)
 Status         : 0x00 (0) (SUCCESS)
 DevAddrType    : 0x00 (0) (ADDRTYPE_PUBLIC)
 DevAddr        : 60:77:71:C7:9F:A2
 ConnHandle     : 0x0000 (0)
 ConnRole       : 0x08 (8) (
                  Central)
 ConnInterval   : 0x0050 (80)
 ConnLatency    : 0x0000 (0)
 ConnTimeout    : 0x07D0 (2000)
 ClockAccuracy  : 0x00 (0)
Dump(Rx):
0000:04 FF 14 05 06 00 00 A2 9F C7 71 77 60 00 00 08 ..........qw`...
0010:50 00 00 00 D0 07 00                            P......
--------------------------------------------------------------------
[16] : <Tx> - 06:48:16.461
-Type           : 0x01 (Command)
-OpCode         : 0x2022 (HCI_LE_SetDataLength)
-Data Length    : 0x06 (6) byte(s)
 Handle         : 0x0000 (0)
 TxOctets       : 0x00FB (251)
 TxTime         : 0x0848 (2120)
Dump(Tx):
0000:01 22 20 06 00 00 FB 00 48 08                   ." .....H.
--------------------------------------------------------------------
[17] : <Info> - 06:48:16.546
Device Connected
Handle = 0x0000
Addr Type = 0x00 (ADDRTYPE_PUBLIC)
BDAddr = 60:77:71:C7:9F:A2
--------------------------------------------------------------------
[18] : <Rx> - 06:48:16.504
-Type           : 0x04 (Event)
-EventCode      : 0x000E (HCI_CommandCompleteEvent)
-Data Length    : 0x06 (6) bytes(s)
 Packets        : 0x01 (1)
 OpCode         : 0x2022 (HCI_LE_SetDataLength)
 Status         : 0x00 (0) (SUCCESS)
 Handle         : 0x0000 (0)
Dump(Rx):
0000:04 0E 06 01 22 20 00 00 00                      ...." ...
--------------------------------------------------------------------
[19] : <Rx> - 06:48:16.767
-Type           : 0x04 (Event)
-EventCode      : 0x003E (HCI_LE_GenericReportEvent)
-Data Length    : 0x0C (12) bytes(s)
 LE Event Code  : 0x04 (4) (HCI_LE_ReadRemoteUsedFeaturesCompleteEvent)
 LE Event Code  : 0x04 (4) (HCI_LE_ReadRemoteUsedFeaturesCompleteEvent)
 Status         : 0x00 (0) (SUCCESS)
 ConnectionId   : 0x0000 (0)
 Features       : 0x00000000000059FF (23039) (
                  Encryption
                  Connection_Parameters_Request
                  Reject_Extended_Indication
                  Slave_Features_Exchange
                  Ping
                  Data_Packet_Length_Extension
                  Privacy
                  Extended_Scanner_Filter_Policies
                  PHY_2M
                  Coded_PHY
                  Extended_Advertising
                  Channel_Selection_Algorithm_2)
Dump(Rx):
0000:04 3E 0C 04 00 00 00 FF 59 00 00 00 00 00 00    .>......Y......
--------------------------------------------------------------------
[20] : <Info> - 06:48:36.968
Device Disconnected
Handle = 0x0000
Addr Type = 0x00 (ADDRTYPE_PUBLIC)
BDAddr = 60:77:71:C7:9F:A2
--------------------------------------------------------------------
[21] : <Rx> - 06:48:36.967
-Type           : 0x04 (Event)
-EventCode      : 0x00FF (HCI_LE_ExtEvent)
-Data Length    : 0x06 (6) bytes(s)
 Event          : 0x0606 (1542) (GAP_TerminateLink)
 Status         : 0x00 (0) (SUCCESS)
 ConnHandle     : 0x0000 (0)
 Reason         : 0x08 (8) (SUPERVISION_TIMEOUT_TERM)
Dump(Rx):
0000:04 FF 06 06 06 00 00 00 08                      .........
--------------------------------------------------------------------

为什么他们无法建立连接?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我的手机能够与 CC2642R2F 建立连接、并成功接收通知

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    感谢您与我们联系。

    由于您成功地在手机和 CC2640R2F 之间建立了稳定的连接、我认为问题可能出在 CC2652R 中。

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!  

    但 CC2652R 项目是主机测试、 我没有做任何更改。 可能是什么问题?

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我怀疑在 CC2652R 上运行的主机测试与在 CC2640R2F 上运行的固件不兼容。  

    我使用 BTool 测试 CC2640R2F 时。 该 BTool 连接到在目标 CC2640R2F 板上运行的同一 SDK 版本的 CC2640R2F Launchpad 并执行主机测试。

    -kel