主题中讨论的其他器件:LP-XDS110ET、 ENERGYTRACE
我希望在禁用广播的情况下、理想情况下 功耗应该会降低、但更确切地说、功耗会增加近13倍。
如果始终启用 BLE 广播、则- 0.1 mA
如果 在 - 1.2 mA 周围始终禁用 BLE 广播
关于
伊兰 

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我希望在禁用广播的情况下、理想情况下 功耗应该会降低、但更确切地说、功耗会增加近13倍。
如果始终启用 BLE 广播、则- 0.1 mA
如果 在 - 1.2 mA 周围始终禁用 BLE 广播
关于
伊兰 

您好!
明白了。 您能否共享测量设置? 要使用 LP-XDS110ET + LP-EM-CC2340R5通过 EnergyTrace 准确测量功率、应执行以下几个步骤:
1.拔下 LED 跳线
2.断开 LP-XDS110ET 和 LP-EM-CC2340R5的连接
3.使用跳线在 LP-XDS110ET 和 LP-EM-CC2340R5之间连接3.3V、GND 和 NRESET
4.独立运行 EnergyTrace
您能否确认这是所使用的设置? 如果可能、您还能分享设置的图片吗?
此致、
1月