This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1352P7:将 Thread 和 BLE 集成到单个映像中

Guru**** 2974170 points

Other Parts Discussed in Thread: LP-CC1352P7, SIMPLELINK-CC13X2-26X2-SDK

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1338179/cc1352p7-integrating-thread-and-ble-into-a-single-image

器件型号:CC1352P7
Thread 中讨论的其他器件: SIMPLELINK-CC13X2-26X2-SDK

您好!

我有两个 LP-CC1352P7开发套件、用于线程功能评估。

当我使用 SIMPLELINK-CC13X2-26X2-SDK 中的线程示例"门锁"时,线程函数工作正常。

现在我想在"Door look"示例中添加 BLE 功能。 我们要使用 BLE 应用将开发套件设置为网关和设备的角色。

我应该从这些示例开始?

如果将 BLE 和 Thread 集成到映像中、是否会出现任何闪存大小问题?

瑞克