This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2640R2F:GAPROLE_STATE 为 GAPROLE_广播、但器件不可发现

Guru**** 2684655 points

Other Parts Discussed in Thread: CC2640R2F, CC2640

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1274437/cc2640r2f-gaprole_state-is-gaprole_advertising-but-device-is-not-discoverable

器件型号:CC2640R2F
主题中讨论的其他器件: CC2640

您好、TI 支持团队、

我将从旧的 BLE Stack "simplelink_cc2640r2_SDK_1_50_00_58"迁移到 CC2640R2F 上的新"simplelink_cc2640r2_SDK_5_30_00_03"和 CCS v12。

我所面临 的问题是每次我芯片启动后,它将保持不可屏蔽的只有15分钟,然后它停止广告,虽然`GAPROLE_STATE,&pValue ) Role_Get`是 GAPROLE_Advertising。

是否有方法可以找到无线电 CPU 的状态? 我试图查看文档、但  找不到可能有用的内容。

谢谢赞赏。
穆罕默