This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2340R5:CC2340R5如何以中心角色开始扫描?

Guru**** 2826755 points

Other Parts Discussed in Thread: CC2340R5

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1372090/cc2340r5-cc2340r5-how-to-start-scan-at-central-role

器件型号:CC2340R5

工具与软件:

您好!

我有一个基于 basic_ble_LP_EM_CC2340R5_freertos_ticlang 示例(Central)的应用程序。 当我从 UART 接收到命令字符串 AT+SCAN\r\n 时、启动扫描之后、程序将跳转到 iCall_abort?

参考文章:

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1278585/cc2340r5-central-to-peripheral-automatically-connect

SDK:simplelink_lowpower_f3_sdk_7_40_00_64

我的代码

/*
 *  ======== callbackFxn ========
 */
void callbackFxn(UART2_Handle handle, void *buffer, size_t count, void *userArg, int_fast16_t status)
{
    if (status != UART2_STATUS_SUCCESS)
    {
        /* RX error occured in UART2_read() */
        while (1) {}
    }


    numBytesRead = count;
    if(scan_state == 0)
         sem_post(&sem);
}
/*
 *  ======== start_scan ========
 */
void start_scan(void)
{
    bStatus_t status;
    const BLEAppUtil_ScanStart_t centralScanStartParams =
    {
         /*! Zero for continuously scanning */
         .scanPeriod     = DEFAULT_SCAN_PERIOD, /* Units of 1.28sec */

         /*! Scan Duration shall be greater than to scan interval,*/
         /*! Zero continuously scanning. */
         .scanDuration   = DEFAULT_SCAN_DURATION, /* Units of 10ms */

         /*! If non-zero, the list of advertising reports will be */
         /*! generated and come with @ref GAP_EVT_SCAN_DISABLED.  */
         .maxNumReport   = APP_MAX_NUM_OF_ADV_REPORTS
    };

    status = BLEAppUtil_scanStart(&centralScanStartParams);

    if(status == FAILURE)
    {
        while(1){}
    }
}
/*
 *  ======== mainThread ========
 */
void *mainThread(void *arg0)
{
    char input;
    const char echoPrompt[] = "Echoing characters:\r\n";
    UART2_Handle uart;
    UART2_Params uartParams;
    int32_t semStatus;
    uint32_t status = UART2_STATUS_SUCCESS;

    /* Call driver init functions */
    GPIO_init();

    /* Configure the LED pin */
    //GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);

    /* Create semaphore */
    semStatus = sem_init(&sem, 0, 0);

    if (semStatus != 0)
    {
        /* Error creating semaphore */
        while (1) {}
    }

    /* Create a UART in CALLBACK read mode */
    UART2_Params_init(&uartParams);
    uartParams.readMode     = UART2_Mode_CALLBACK;
    uartParams.readCallback = callbackFxn;
    uartParams.baudRate     = 115200;

    uart = UART2_open(CONFIG_DISPLAY_UART, &uartParams);

    if (uart == NULL)
    {
        /* UART2_open() failed */
        while (1) {}
    }

    /* Turn on user LED to indicate successful initialization */
    //GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_ON);

    /* Pass NULL for bytesWritten since it's not used in this example */
    UART2_write(uart, echoPrompt, sizeof(echoPrompt), NULL);

    /* Loop forever echoing */
    while (1)
    {
      switch(scan_state)
      {
       case 0:

           numBytesRead = 0;


           /* Pass NULL for bytesRead since it's not used in this example */
           status = UART2_read(uart, &input, 1, NULL);

           if (status != UART2_STATUS_SUCCESS)
           {
               /* UART2_read() failed */
               while (1) {}
           }

           /* Do not write until read callback executes */
           sem_wait(&sem);


           if (numBytesRead > 0)
           {
               ch_buffer[ch_cnt++] = (uint8_t)input;

               if(strstr((const char *)ch_buffer,(const char *)"\r\n" ) != 0)
               {

                   if(strcmp((const char *)ch_buffer,(const char *)"AT+SCAN\r\n") == 0 )
                   {
                       scan_state =  1;

                       status = UART2_write(uart, (const char *)"Msg:success:", strlen((const char *)"Msg:success:"), NULL);

                   }
                   else{
                       status = UART2_write(uart, (const char *)"ack:", strlen((const char *)"ack:"), NULL);
                   }

                   status = UART2_write(uart, (const char *)ch_buffer, strlen((const char *)ch_buffer), NULL);
                   if (status != UART2_STATUS_SUCCESS)
                   {
                           /* UART2_write() failed */
                        while (1) {}
                   }


                   void *ptr = (void *)ch_buffer;
                   memset(ptr,0,100);
                   ch_cnt = 0;

               }
           }
           break;
           case 1:
               start_scan();
               scan_state =  2;
           break;

        }


    }
}

ICall 中断

/**
 * Aborts.
 *
 * This is preferred over C runtime abort() function,
 * in an external image since the C runtime abort() is only
 * guaranteed in a root image which contains the C runtime
 * entry function that is executed upon startup.
 */
ICall_Errno
ICall_abort(void)
{
#ifdef HALNODEBUG
#elif  defined(EXT_HAL_ASSERT)
  HAL_ASSERT(HAL_ASSERT_CAUSE_ICALL_ABORT);
#else
  {
    volatile uint8_t j=1;
    while(j);
  }
#endif /* EXT_HAL_ASSERT */
  ICALL_HOOK_ABORT_FUNC();
  return(ICALL_ERRNO_SUCCESS);
}