This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2340R5-Q1:连接监视器是否具有时间同步功能

Guru**** 2589280 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1379489/cc2340r5-q1-whether-the-connection-monitor-has-a-time-synchronization-function

器件型号:CC2340R5-Q1

工具与软件:

您好、TI

连接监视器是否支持时间同步? 如果支持它、我如何实现它?

我从代码中看到、当前的方式是计算 deltaTime 以及一些 参数(如 BUS_LATENCY_IN_MS)要跳过的通道数。

// With a 100ms connection interval we will skip 3 channels into the future (in each connection event we can monitor 1 channel)
    // This is mainly done to ensure that even a very slow bus is able to send the connection information in time
    // In time: before the Central/Peripheral already go past the channel that we chose to listen on
    // If Central/Peripheral are already past this point, we will have to wait numChannels*connInterval until we catch the
    // connection once again
    chanSkip = (uint16_t)((BUS_LATENCY_IN_MS/connInterval) + 1);

    // DeltaTime is the distance between the current time and time we received the data for the new connection.
    deltaTime = uble_timeDelta(currTime, reqTime);

    // Figure out how many connection events have passed since the last anchor point
    if (deltaTime > connInterval * BLE_TO_RAT)
    {
      chanReqDiff = (uint16_t) (deltaTime / (connInterval * BLE_TO_RAT) + 1);
    }

    if (gUpdateSessionMissEvents[hostConnHandle] == 0)
    {
      ubCMConnInfo.ArrayOfConnInfo[i].currentChan = setNextDataChan(sessionId, chanSkip + chanReqDiff); //jump some [ms] channels into the future
      // Catch anchor point n+2 connection intervals in the future
      ubCMConnInfo.ArrayOfConnInfo[i].scanDuration = (uint16_t)(connInterval*(chanSkip +chanReqDiff+1));
    }
    else //gUpdateSessionMissEvents[hostConnHandle] != 0
    {
      // Indicates that there was a Connection param update of an active connection handle, then take into consideration the calculation of num events missed until the new param update.
      ubCMConnInfo.ArrayOfConnInfo[i].currentChan = setNextDataChan(sessionId, gUpdateSessionMissEvents[hostConnHandle] + chanReqDiff);
      ubCMConnInfo.ArrayOfConnInfo[i].scanDuration = (uint16_t)(connInterval*(chanSkip +1));
    }

这将导致在使用较慢的总线时有时无法进行监控。 我也不确定对于慢速总线、BUS_LATENCY_IN_MS 的值应该是多少。

是否有办法解决这个问题(例如时间同步)? 例如、NXP 的产品在传输连接参数之前执行时间同步。

此致

普雷斯顿

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、TI

    有任何这方面的信息吗?

    此致

    普雷斯顿