This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2745P10-Q1:连接到 BLE 时处理 ICall 任务

Guru**** 2578945 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1442543/cc2745p10-q1-processing-of-icall-task-when-connected-to-ble

器件型号:CC2745P10-Q1

工具与软件:

我检查了 ICall 任务在 BLE 连接期间运行的时间、发现任务在接下来的时间已被占用1~3ms。
每一项的处理时间是多少?

  1. 建立 BLE 连接时、此任务占用大约3ms。


  2. BLE 连接后、每60ms 执行一次任务、大约1ms。