This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2541:了解 BLE 数据传输、UUID、AT 命令和应用开发(使用 CC2541)

Guru**** 2994400 points

Other Parts Discussed in Thread: CC2541, CC2340R5

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1463754/cc2541-understanding-ble-data-transmission-uuids-at-commands-and-application-development-with-cc2541

器件型号:CC2541
主题中讨论的其他器件: CC2340R5

工具与软件:

尊敬的 TI 团队:

我目前使用的是 CC2541 IC、对于其运行以及应用开发指南有一些问题:

  1. BLE 数据传输 :

    • 当一个字符从微控制器发送到 CC2541时、IC 如何将该数据帧到 BLE 结构中以便进行传输?
    • 您能否简要说明 BLE 堆栈在此过程中的作用?
  2. UUID 功能 :

    • UUID 在 BLE 通信中的重要性是什么、如何使用它们来区分服务和特征?
  3. AT 命令机制 :

    • AT 命令如何在 CC2541的内部工作以配置和控制其运行?
    • 具体而言、固件如何解释和处理这些命令?
  4. 应用开发 :

    • 我们计划开发自定义 BLE 应用、该应用包括连接和断开与基于 CC2541的器件的连接、以及发送和接收数据等功能。 您能否提供实施这些功能的指导或最佳实践?

您的见解将帮助我们更好地了解 CC2541的运行、并帮助我们创建强大的 BLE 应用。

提前感谢您的支持!

此致、
Ajith Kumar