This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28027F:TMS320F28027F

Guru**** 2595805 points
Other Parts Discussed in Thread: C2000WARE, LAUNCHXL-F28027F, TMS320F28027F

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1495601/tms320f28027f-tms320f28027f

器件型号:TMS320F28027F
主题中讨论的其他器件:LAUNCHXL-F28027F、C2000WARE、 ENERGIA

工具/软件:

有没有人可以帮助我使用 C2000 Piccolo 的 bmp 传感器在 i2c 接口上工作 Launchxl-f28027f 我已经尝试了许多方法没有得到请检查  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Kishor:

    作为起点、您可以参考 I2C EEPROM 示例作为与传感器连接的起点。 如果您对实施有任何具体问题、请告诉我、我可以提供帮助。

    C:\ti\c2000\C2000Ware_5_04_00_00\device_support\F2802x\examples\structs\i2c_EEPROM

    此致、

    Aishwarya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Aishwarya Rajesh

    "我已经编写了使用 I2C 将 BMP280传感器与 TMS320F28027F 连接的逻辑、但我无法获得任何输出。 请看一下代码、让我知道可能有什么问题。"

    #include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
    #include <stdio.h>              // For sprintf
    #include <stdint.h>             // For uint8_t, int16_t, etc.
    
    // BMP280 Definitions
    #define BMP280_ADDR 0x76        // BMP280 I2C address (0x76 if SDO is low, 0x77 if SDO is high)
    #define BMP280_CALIB_DATA_SIZE 24
    
    // BMP280 Calibration Data
    uint16_t dig_T1;
    int16_t dig_T2, dig_T3;
    uint16_t dig_P1;
    int16_t dig_P2, dig_P3, dig_P4, dig_P5, dig_P6, dig_P7, dig_P8, dig_P9;
    
    // Global variable for fine temperature calculation
    int32_t t_fine;
    
    // Function Prototypes
    void InitI2C(void);
    void BMP280_Init(void);
    void I2C_Write(uint8_t slave_addr, uint8_t reg_addr, uint8_t data);
    void I2C_Read(uint8_t slave_addr, uint8_t reg_addr, uint8_t *data, uint8_t length);
    void BMP280_ReadCalibrationData(void);
    void BMP280_ReadData(float *temperature, float *pressure);
    float compensate_T(int32_t adc_T);
    float compensate_P(int32_t adc_P);
    void InitSCI(void);
    void SCI_Print(char *str);
    
    // Main Function
    void main(void)
    {
        float temperature, pressure;
        char buffer[50];  // Buffer to store formatted strings
    
        // Initialize system
        InitSysCtrl();      // Initialize the system control
        InitI2C();          // Initialize I2C for BMP280 communication
        InitSCI();          // Initialize SCI for UART communication
    
        // Test UART communication
        SCI_Print("Hello, BMP280!\n");
    
        // Initialize BMP280 sensor
        BMP280_Init();
        BMP280_ReadCalibrationData();  // Read calibration data from BMP280
    
        while (1)
        {
            // Read temperature and pressure from BMP280
            BMP280_ReadData(&temperature, &pressure);
    
            // Format and send temperature data
            sprintf(buffer, "Temperature: %.2f °C\n", temperature);
            SCI_Print(buffer);
    
            // Format and send pressure data
            sprintf(buffer, "Pressure: %.2f Pa\n", pressure);
            SCI_Print(buffer);
    
            DELAY_US(1000000);  // Delay for 1 second
        }
    }
    
    // Initialize I2C module
    void InitI2C(void)
    {
        // Enable I2C peripheral clock
        SysCtrlRegs.PCLKCR0.bit.I2CAENCLK = 1;
    
        // Configure I2C pins (GPIO32 as SDA and GPIO33 as SCL)
        EALLOW;
        GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0;    // Enable pull-up for SDA (GPIO32)
        GpioCtrlRegs.GPBPUD.bit.GPIO33 = 0;    // Enable pull-up for SCL (GPIO33)
        GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 1;   // Configure GPIO32 as I2C SDA
        GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 1;   // Configure GPIO33 as I2C SCL
        EDIS;
    
        // Initialize I2C
        I2caRegs.I2CMDR.all = 0x0000;          // Put I2C in reset state
        I2caRegs.I2CPSC.all = 6;               // Prescaler for 12.5 MHz SYSCLK
        I2caRegs.I2CCLKL = 10;                 // Low time = 10 * I2CPSC
        I2caRegs.I2CCLKH = 10;                 // High time = 10 * I2CPSC
        I2caRegs.I2CMDR.all = 0x0020;          // Master mode, 7-bit address, free data format
    }
    
    // Initialize BMP280 sensor
    void BMP280_Init(void)
    {
        // Set oversampling and mode
        I2C_Write(BMP280_ADDR, 0xF4, 0x27);  // Control measurement register: x1 temp, x1 pressure, normal mode
        I2C_Write(BMP280_ADDR, 0xF5, 0x00);  // Configuration register: filter off, standby time 0.5ms
    }
    
    // Write to BMP280 register
    void I2C_Write(uint8_t slave_addr, uint8_t reg_addr, uint8_t data)
    {
        I2caRegs.I2CSAR = slave_addr;          // Set slave address
        I2caRegs.I2CCNT = 2;                   // Set byte count (register address + data)
        I2caRegs.I2CDXR = reg_addr;            // Load register address
        I2caRegs.I2CDXR = data;                // Load data
        I2caRegs.I2CMDR.all = 0x6E20;          // Start condition, master transmitter mode
    
        uint16_t timeout = 10000;              // Timeout counter
        while (I2caRegs.I2CSTR.bit.ARDY == 0 && timeout--); // Wait for stop condition
        if (timeout == 0) {
            SCI_Print("I2C Write Timeout!\n");
        }
    }
    
    // Read from BMP280 register
    void I2C_Read(uint8_t slave_addr, uint8_t reg_addr, uint8_t *data, uint8_t length)
    {
        I2caRegs.I2CSAR = slave_addr;          // Set slave address
        I2caRegs.I2CCNT = 1;                   // Set byte count for register address
        I2caRegs.I2CDXR = reg_addr;            // Load register address
        I2caRegs.I2CMDR.all = 0x6E20;          // Start condition, master transmitter mode
    
        uint16_t timeout = 10000;              // Timeout counter
        while (I2caRegs.I2CSTR.bit.ARDY == 0 && timeout--); // Wait for stop condition
        if (timeout == 0) {
            SCI_Print("I2C Read Address Timeout!\n");
        }
    
        I2caRegs.I2CCNT = length;              // Set byte count for data
        I2caRegs.I2CMDR.all = 0x2C20;          // Start condition, master receiver mode
    
        unsigned char i;  // Declare loop variable
        for (i = 0; i < length; i++) {
            timeout = 10000;                    // Reset timeout for each byte
            while (I2caRegs.I2CSTR.bit.RRDY == 0 && timeout--); // Wait for receive ready
            if (timeout == 0) {
                SCI_Print("I2C Read Data Timeout!\n");
                break;
            }
            data[i] = I2caRegs.I2CDRR;         // Read data
        }
    }
    
    // Read BMP280 calibration data
    void BMP280_ReadCalibrationData(void)
    {
        uint8_t calib_data[BMP280_CALIB_DATA_SIZE];
        I2C_Read(BMP280_ADDR, 0x88, calib_data, BMP280_CALIB_DATA_SIZE);
    
        dig_T1 = (calib_data[1] << 8) | calib_data[0];
        dig_T2 = (calib_data[3] << 8) | calib_data[2];
        dig_T3 = (calib_data[5] << 8) | calib_data[4];
        dig_P1 = (calib_data[7] << 8) | calib_data[6];
        dig_P2 = (calib_data[9] << 8) | calib_data[8];
        dig_P3 = (calib_data[11] << 8) | calib_data[10];
        dig_P4 = (calib_data[13] << 8) | calib_data[12];
        dig_P5 = (calib_data[15] << 8) | calib_data[14];
        dig_P6 = (calib_data[17] << 8) | calib_data[16];
        dig_P7 = (calib_data[19] << 8) | calib_data[18];
        dig_P8 = (calib_data[21] << 8) | calib_data[20];
        dig_P9 = (calib_data[23] << 8) | calib_data[22];
    }
    
    // Read temperature and pressure data from BMP280
    void BMP280_ReadData(float *temperature, float *pressure)
    {
        uint8_t data[6];
        I2C_Read(BMP280_ADDR, 0xF7, data, 6); // Read pressure and temperature data
    
        int32_t adc_P = (data[0] << 12) | (data[1] << 4) | (data[2] >> 4);
        int32_t adc_T = (data[3] << 12) | (data[4] << 4) | (data[5] >> 4);
    
        *temperature = compensate_T(adc_T);
        *pressure = compensate_P(adc_P);
    }
    
    // Temperature compensation formula
    float compensate_T(int32_t adc_T)
    {
        int32_t var1, var2;
        var1 = ((((adc_T >> 3) - ((int32_t)dig_T1 << 1))) * ((int32_t)dig_T2)) >> 11;
        var2 = (((((adc_T >> 4) - ((int32_t)dig_T1)) * ((adc_T >> 4) - ((int32_t)dig_T1))) >> 12) * ((int32_t)dig_T3)) >> 14;
        t_fine = var1 + var2;  // Update t_fine for pressure compensation
        return (t_fine * 5 + 128) >> 8;  // Return temperature in °C
    }
    
    // Pressure compensation formula
    float compensate_P(int32_t adc_P)
    {
        int64_t var1, var2, p;
        var1 = ((int64_t)t_fine) - 128000;
        var2 = var1 * var1 * (int64_t)dig_P6;
        var2 = var2 + ((var1 * (int64_t)dig_P5) << 17);
        var2 = var2 + ((int64_t)dig_P4 << 35);
        var1 = ((var1 * var1 * (int64_t)dig_P3) >> 8) + ((var1 * (int64_t)dig_P2) << 12);
        var1 = (((int64_t)1 << 47) + var1) * ((int64_t)dig_P1) >> 33;
        if (var1 == 0) return 0;  // Avoid division by zero
        p = 1048576 - adc_P;
        p = (((p << 31) - var2) * 3125) / var1;
        var1 = ((int64_t)dig_P9 * (p >> 13) * (p >> 13)) >> 25;
        var2 = ((int64_t)dig_P8 * p) >> 19;
        p = ((p + var1 + var2) >> 8) + ((int64_t)dig_P7 << 4);
        return (float)p / 256.0;  // Return pressure in Pa
    }
    
    // Initialize SCI for UART communication
    void InitSCI(void)
    {
        // Enable SCI peripheral clock
        SysCtrlRegs.PCLKCR0.bit.SCIAENCLK = 1;
    
        // Configure SCI pins
        EALLOW;
        GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0;    // Enable pull-up for SCITXDA (GPIO28)
        GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0;    // Enable pull-up for SCIRXDA (GPIO29)
        GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1;   // Configure GPIO28 as SCITXDA
        GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1;   // Configure GPIO29 as SCIRXDA
        EDIS;
    
        // Initialize SCI
        SciaRegs.SCICCR.all = 0x0007;  // 1 stop bit, no parity, 8-bit data, idle-line protocol
        SciaRegs.SCICTL1.all = 0x0003; // Enable TX and RX, internal SCICLK
        SciaRegs.SCIHBAUD = 0x0001;    // Baud rate = 9600 (for 12.5 MHz SYSCLK)
        SciaRegs.SCILBAUD = 0x00E7;
        SciaRegs.SCICTL1.all = 0x0023; // Relinquish SCI from reset
    }
    
    // Print a string via SCI
    void SCI_Print(char *str)
    {
        while (*str) {
            while (SciaRegs.SCICTL2.bit.TXRDY == 0); // Wait for TX ready
            SciaRegs.SCITXBUF = *str++;               // Send character
        }
    }
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Kishor、

    虽然我无法查看代码、但请告诉我您是否 在 GPIO 上看到任何输出、或者根本不看到任何输出? 如果引脚上没有输出、请查看 GPIO 配置以及 MCU 与 EEPROM 之间的物理连接。 如果有输出、那么我们可以进一步查看代码配置。 请指出代码的特定部分可能存在问题。

    以下 是一个 相关的主题: (+) TMS320F28027F:I2C 在不收到命令的情况下设置停止条件- C2000微控制器论坛- C2000Tm︎ 微控制器- TI E2E 支持论坛。 论坛上还有其他 E2E 可能 会有所帮助。

    此致、

    Aishwarya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Kishor、

    您能否确认在示波器上是否看到任何输出并分享所看到的内容。 我不清楚这一点。 此外、确保您有一个阻值约为2.2k Ω 的上拉电阻将 SDA 和 SCL 连接到 VDDIO。 有关更多信息、也请参阅此应用手册: 使用 C2000 I2C 模块连接 EEPROM

    还请给我1-2天时间来进一步研究这个问题、并返回给您。  

    此致、

    Aishwarya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Aishwarya Rajesh:

    我使用4.7千欧  上拉电阻将 SDA 和 SCL 连接到 VCC。

    输出 iAM 看到

    在 bmp_low_level.c 中、读取操作超时

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Kishor、

    您能否在示波器上发送读数图像。

    此致、

    Aishwarya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Aishwarya Rajesh:

    已查看逻辑分析仪  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Kishor、

    让我再深入研究一下、然后再联系您。

    此致、

    Aishwarya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Kishor、

    请尝试参考这些主题、如果您有任何其他问题、请告诉我:  

    28027F 通过 I2C 进行外部控制-电机控制

    CCS/LAUNCHXL-F28027:如何在 LAUNCHXL-F28027和 MCP9808之间建立 I2C 通信?

    此致、

    Aishwarya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Aishwarya Rajesh:

    感谢这个响应,我已经检测到 bmp280传感器芯片 ID (检测到 i2c )通过这个线程,现在工作获取 bmp 传感器数据,如果有任何问题,我会得到你。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Kishor、

    很高兴听到这个消息、如果您有任何其他问题、请告诉我、和/或请将此主题标记为已相应解决。

    此致、

    Aishwarya