- 器件型号:TMS320F28379D
尊敬的 TI:
我对嵌套中断有疑问。 我使用 C2000示例学习这一点、因为直接从我的项目中我无法运行我的理论。 这个问题的目的是确认一个 User1中断是否可被另一个中断中断中断中断中断。
User1中断是不可屏蔽的中断、这意味着如果执行了_asm (" trap #number)、CPU 将到达它的任何情况下、该中断是否可以通过其他外设的更高中断来中断?
为了进行本实验、我在 c2000ware 中对 swperped_interrupts_cpu01项目添加了一些小的修改。如果需要、您可以从您的角度执行同样的操作、因此我将使用此示例。
首先、我在该文件 SWPrioritizeDefaultIsr.c 中向 User1 ISR 添加了一些代码:
//
// Connected to USER1 of CPU (non-maskable):
//
__interrupt void USER1_ISR(void) // User Defined trap 1
{
EINT;
//
// Insert ISR Code here.......
//
for(i = 1; i <= 100; i++) {}
// Next two lines for debug only to halt the processor here
// Remove after inserting ISR Code
// __asm (" ESTOP0");
// for(;;);
//
// Add ISR to Trace
//
ISRTrace[ISRTraceIndex] = 0xCA01;
ISRTraceIndex++;
}
for 循环比其他中断服务例程中的 for 循环长10倍。 我的目标是查看此中断服务例程是否会嵌套具有最高优先级的中断。
其次、我在 PieCtrlRegs.PIEIFR1.all = ISRs_Group1之后和之前运行__asm (" trap #20")指令:
//
// CASE 1:
//
#if (CASE==1)
//
// Force all group 1 interrupts at once by writing to the PIEIFR1
// register
//
//
// Prepare for the test:
// Disable interrupts
// Clear the trace buffer, PIE Control Register, CPU IER and IFR
// registers
//
DINT;
for(i = 0; i < 50; i++)
{
ISRTrace[i] = 0;
}
ISRTraceIndex = 0;
InitPieCtrl();
IER = 0;
IFR &= 0;
//
// Enable the PIE block
//
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
//
// Enable PIE group 1 interrupt 1-8
//
PieCtrlRegs.PIEIER1.all = 0x00FF;
//
// Make sure PIEACK for group 1 is clear (default after reset)
//
PieCtrlRegs.PIEACK.all = M_INT1;
//
// Enable CPU INT1
//
IER |= M_INT1;
//
// Force all valid interrupts for Group 1
//
__asm(" TRAP #20");
PieCtrlRegs.PIEIFR1.all = ISRS_GROUP1;
//
// Enable global Interrupts CPU level:
//
EINT; // Enable Global interrupt INTM
//
// Wait for all Group 1 interrupts to be serviced
//
while(PieCtrlRegs.PIEIFR1.all != 0x0000 ){}
//
// Stop here and check the ISRTrace to determine which order the
// ISR Routines completed. The order is dependant on the priority
// assigned in the F2837xD_SWPrioritizedIsrLevels.h file
//
// The ISRTrace will contain a list of values corresponding to the
// interrupts serviced in the order they were serviced.
// For example if the ISRTrace looks like this
// 0x0014 ISR Group 1 interrupt 4
// 0x0017 ISR Group 1 interrupt 7
// 0x0016 ISR Group 1 interrupt 6
// 0x0015 ISR Group 1 interrupt 5
// 0x0018 ISR Group 1 interrupt 8
// 0x0012 ISR Group 1 interrupt 2
// 0x0011 ISR Group 1 interrupt 1
// 0x0000 end of trace
//
__asm(" ESTOP0");
我正在执行示例的第一个示例。
我使用 的 F2837xD_SWPrioritizedIsrLevels.h 与 TI 相同:
#define INT1PL 2 // Group1 Interrupts (PIEIER1) #define INT2PL 1 // Group2 Interrupts (PIEIER2) #define INT3PL 4 // Group3 Interrupts (PIEIER3) #define INT4PL 2 // Group4 Interrupts (PIEIER4) #define INT5PL 2 // Group5 Interrupts (PIEIER5) #define INT6PL 3 // Group6 Interrupts (PIEIER6) #define INT7PL 5 // Group7 Interrupts (PIEIER6) #define INT8PL 5 // Group8 Interrupts (PIEIER6) #define INT9PL 3 // Group9 Interrupts (PIEIER9) #define INT10PL 6 // Group10 Interrupts (PIEIER6) #define INT11PL 6 // Group11 Interrupts (PIEIER6) #define INT12PL 8 // Group12 Interrupts (PIEIER6) #define INT13PL 4 // XINT13 #define INT14PL 4 // INT14 (TINT2) #define INT15PL 4 // DATALOG #define INT16PL 4 // RTOSINT ... #define G1_1PL 5 // ADCA1_INT #define G1_2PL 3 // ADCB1_INT #define G1_3PL 1 // ADCC1_INT #define G1_4PL 4 // XINT1_INT #define G1_5PL 4 // XINT2_INT #define G1_6PL 1 // ADCD1_INT #define G1_7PL 12 // TIMER0_INT #define G1_8PL 5 // WAKE_INT #define G1_9PL 0 // Reserved #define G1_10PL 0 // Reserved #define G1_11PL 0 // Reserved #define G1_12PL 0 // Reserved #define G1_13PL 8 // IPC1_INT #define G1_14PL 13 // IPC2_INT #define G1_15PL 15 // IPC3_INT #define G1_16PL 9 // IPC4_INT
结果:

在这张图片中、我们可以看到、即使 #define G1_3PL 1 // ADCC1_INT 是最高优先级、用户1中断也会获得执行的第一个中断?
用户中断到达 ADCC1_INT 时是否中断? 我不确定 User1中断是否嵌套了高优先级、我认为即使我们定义了最高优先级中断、当用户中断开始执行时、它也不会停止、直到结束和其他最高优先级处于挂起状态。
请您澄清这一点吗?
提前感谢您、
此致、
S.Tarik