This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28377S:具有死区时间的 HRPWM 上行-下行

Guru**** 2614265 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1015095/tms320f28377s-hrpwm-up-down-with-dead-time

器件型号:TMS320F28377S

Hallo、

我需要扩展现有的 ePWM 配置。 我们基于3个同步的 ePWM 实现了 FOC。

周期和死区时间设置为一次且永不改变、CMPAx 用于占空比。 输出 EPWMxB 反相 EPWMxA。

CMPAx 的影子寄存器在单次触发模式下全局加载。

此外  、SOC_A 由 PWM2:CMPB 触发。 该计时是恒定的。

问题:

CAMPHR 已正确更新在调试器视图中可以看到的内容。 遗憾的是、在输出信号(示波器)中未看到任何结果。 它仍可用作无 HR 扩展的 ePWM。

当我添加 HRPWM 配置函数时、死区时间似乎消失了。 如果我完全删除死区时间支持、那么 HRPWM 将正常工作。

    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM1);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM2);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM3);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_HRPWM); //sourced from ePWM1 clock source

    while  (m_sfo_status == SFO_INCOMPLETE) // Call until complete
    {
        m_sfo_status = SFO();
        if (m_sfo_status == SFO_ERROR)
        {
            ESTOP0;    // SFO function returns 2 if an error occurs and number of MEP steps/coarse step exceeds maximum of 255.
        }
    }

    // Disable sync(Freeze clock to PWM as well)
    SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_GTBCLKSYNC);
    SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);

    // ePWM1 - master
    GPIO_setPadConfig(145, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_145_EPWM1A); // phase UH
    GPIO_setPadConfig(146, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_146_EPWM1B);
   // ePWM2
    GPIO_setPadConfig(147, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_147_EPWM2A); // phase VH
    GPIO_setPadConfig(148, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_148_EPWM2B);
    // ePWM3
    GPIO_setPadConfig(149, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_149_EPWM3A);
    GPIO_setPadConfig(150, GPIO_PIN_TYPE_STD);
    GPIO_setPinConfig(GPIO_150_EPWM3B);

    // master PWM gets no phase shift
    set_ePWM_config( EPWM1_BASE, m_period, 0, deadband_delay_rising_edge_in_ticks, deadband_delay_falling_edge_in_ticks );
    // slave PWMs get always phase shift 2
    set_ePWM_config( EPWM2_BASE, m_period, 2, deadband_delay_rising_edge_in_ticks, deadband_delay_falling_edge_in_ticks );
    set_ePWM_config( EPWM3_BASE, m_period, 2, deadband_delay_rising_edge_in_ticks, deadband_delay_falling_edge_in_ticks );

    EPWM_setSyncOutPulseMode(EPWM1_BASE, EPWM_SYNC_OUT_PULSE_ON_COUNTER_ZERO); // EPWM 1 is master and olny sync generator
    EPWM_setSyncOutPulseMode(EPWM2_BASE, EPWM_SYNC_OUT_PULSE_ON_EPWMxSYNCIN); // slave
    EPWM_setSyncOutPulseMode(EPWM3_BASE, EPWM_SYNC_OUT_PULSE_ON_EPWMxSYNCIN); // slave

    // ADC trigger offset (EPWM_COUNTER_COMPARE_B)
    EPWM_setCounterCompareValue(EPWM2_BASE, EPWM_COUNTER_COMPARE_B, ( adc_trigger_pmwcount ));
    EPWM_setADCTriggerSource(EPWM2_BASE, EPWM_SOC_A, EPWM_SOC_TBCTR_U_CMPB);
    EPWM_setADCTriggerEventPrescale(EPWM2_BASE, EPWM_SOC_A, 1);
    EPWM_enableADCTrigger(EPWM2_BASE, EPWM_SOC_A);
    EPWM_setCounterCompareShadowLoadMode( EPWM2_BASE,
                                          EPWM_COUNTER_COMPARE_B,
                                          EPWM_COMP_LOAD_ON_CNTR_ZERO);

    // Enable global shadow to active load for CMPA registers. See TRM 13.4.7.2 "One-Shot Load Mode"
    EPWM_enableGlobalLoad(EPWM1_BASE);  //GLDCTL[GLD]=1, individual shadowing is ignored
    EPWM_enableGlobalLoadOneShotMode(EPWM1_BASE); // GLDCTL[OSHTMODE] enable one-shot
    EPWM_enableGlobalLoadRegisters(EPWM1_BASE, EPWM_GL_REGISTER_CMPA_CMPAHR); // GLDCFG - register to be shadow-loaded
    EPWM_setGlobalLoadTrigger(EPWM1_BASE, EPWM_GL_LOAD_PULSE_CNTR_PERIOD); //load on CNT_ZERO - GLDCTL[GLDMODE]
    EPWM_setupEPWMLinks(EPWM1_BASE, EPWM_LINK_WITH_EPWM_3, EPWM_LINK_GLDCTL2); //writing to ePWM3 (one shot trigger) causes writing trigger (the same value of GLDCTL2) to ePWM1

    EPWM_enableGlobalLoad(EPWM2_BASE);
    EPWM_enableGlobalLoadOneShotMode(EPWM2_BASE);
    EPWM_enableGlobalLoadRegisters(EPWM2_BASE, EPWM_GL_REGISTER_CMPA_CMPAHR);
    EPWM_setGlobalLoadTrigger(EPWM2_BASE, EPWM_GL_LOAD_PULSE_CNTR_PERIOD);
    EPWM_setupEPWMLinks(EPWM2_BASE, EPWM_LINK_WITH_EPWM_3, EPWM_LINK_GLDCTL2); //writing to ePWM3 (one shot trigger) causes writing trigger to ePWM1

    EPWM_enableGlobalLoad(EPWM3_BASE);
    EPWM_enableGlobalLoadOneShotMode(EPWM3_BASE);
    EPWM_enableGlobalLoadRegisters(EPWM3_BASE, EPWM_GL_REGISTER_CMPA_CMPAHR);
    EPWM_setGlobalLoadTrigger(EPWM3_BASE, EPWM_GL_LOAD_PULSE_CNTR_PERIOD);

    // see Technical Reference page 1566: should be enabled after all ePWMs are initialized
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_GTBCLKSYNC);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
	
	
	
	
	
void set_ePWM_config(uint32_t epwm_base, uint16_t period, uint16_t offset, uint16_t deadband_delay_rising_edge, uint16_t deadband_delay_falling_edge)
{
    // Set-up TBCLK
    EPWM_setPeriodLoadMode(epwm_base, EPWM_PERIOD_DIRECT_LOAD); //direct load and never change, shadow is not used for period
    EPWM_setTimeBasePeriod(epwm_base, period);
    EPWM_setPhaseShift(epwm_base, offset);
    EPWM_setTimeBaseCounter(epwm_base, offset);
    EPWM_setEmulationMode(epwm_base, EPWM_EMULATION_FREE_RUN);

    // Set up counter mode
    EPWM_setTimeBaseCounterMode(epwm_base, EPWM_COUNTER_MODE_UP_DOWN);

    EPWM_setClockPrescaler(epwm_base,EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1);

    // if offset == 0 then there is master ePWM
    if( 0 == offset )
    {
        EPWM_disablePhaseShiftLoad(epwm_base);
//        HRPWM_disablePhaseShiftLoad(epwm_base);
    }
    else
    {
        EPWM_enablePhaseShiftLoad(epwm_base);
        EPWM_setCountModeAfterSync(epwm_base, EPWM_COUNT_MODE_UP_AFTER_SYNC);
    }
//    HRPWM_selectPeriodLoadEvent(epwm_base, EPWM_SHADOW_LOAD_MODE_SYNC); //load shadow when sync happens, TODO: no one wants to reload period register
//    HRPWM_setCounterCompareShadowLoadEvent(epwm_base, HRPWM_CHANNEL_A, HRPWM_LOAD_ON_CNTR_PERIOD); //slaves do not reach CNTR==0 because of phase shift --check it!
    // Set actions
    EPWM_setActionQualifierAction(epwm_base,
                                  EPWM_AQ_OUTPUT_A,
                                  EPWM_AQ_OUTPUT_HIGH,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
    // down counting: Output A low
    EPWM_setActionQualifierAction(epwm_base,
                                  EPWM_AQ_OUTPUT_A,
                                  EPWM_AQ_OUTPUT_LOW,
                                  EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);

    // enable rising and falling edge delay (S0, S1)
    EPWM_setDeadBandDelayMode(epwm_base, EPWM_DB_RED, true);
    EPWM_setDeadBandDelayMode(epwm_base, EPWM_DB_FED, true);
    // set EPWM_A as "lead" signal (S4, S5)
    EPWM_setRisingEdgeDeadBandDelayInput(epwm_base, EPWM_DB_INPUT_EPWMA);
    EPWM_setFallingEdgeDeadBandDelayInput(epwm_base, EPWM_DB_INPUT_EPWMA);
    // invert output logic of B, don't invert A (S2, S3)
    EPWM_setDeadBandDelayPolarity(epwm_base, EPWM_DB_RED, EPWM_DB_POLARITY_ACTIVE_HIGH);
    EPWM_setDeadBandDelayPolarity(epwm_base, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_LOW);
    // set output swapping of out_A/out_B (S6, S7)
    EPWM_setDeadBandOutputSwapMode(epwm_base, EPWM_DB_OUTPUT_A, true);
    EPWM_setDeadBandOutputSwapMode(epwm_base, EPWM_DB_OUTPUT_B, true);
    // set delay counts
    EPWM_setFallingEdgeDelayCount(epwm_base, deadband_delay_falling_edge);
    EPWM_setRisingEdgeDelayCount(epwm_base, deadband_delay_rising_edge);

//    HRPWM_disablePeriodControl(epwm_base);
    HRPWM_setMEPControlMode(epwm_base, HRPWM_CHANNEL_A, HRPWM_MEP_DUTY_PERIOD_CTRL); //MEP controlled by value of CMPA
    HRPWM_setMEPEdgeSelect(epwm_base, HRPWM_CHANNEL_A, HRPWM_MEP_CTRL_RISING_AND_FALLING_EDGE);

    HRPWM_setDeadbandMEPEdgeSelect(epwm_base, HRPWM_DB_MEP_CTRL_RED_FED);
//    HRPWM_setChannelBOutputPath(epwm_base, HRPWM_OUTPUT_ON_B_INV_A); //dead time is overwritten?
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    此线程与 另一个线程重复。 我将此主题标记为已解决以关闭此主题。 我们可以在另一个线程中解决您的问题。

    谢谢、

    Aditya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您能否将另一个主题与可能的解决方案链接起来?