主题中讨论的其他器件:UNIFLASH
我们目前正在尝试在生产中实现串行闪存编程器功能。 但是、我们很难将固件的生产版本上传到处理器。
当我们在输出十六进制文件中包含设置 DCSM 密码的功能时。 我们会得到校验和错误或空白错误(如果处理器已预编程)。 这是我们要包含的文件(除了密码文件本身)、我们似乎找不到导致问题的任何特定内容。 如果我们编译到.out 文件并使用 UniFlash 将其发送到处理器、则一切正常。
/* this linker command file is to be included if user wants to use the DCSM feature on the device
* DCSM means Dual Zone Code Security Module.
* This linker command file works as an addendum ot the already existing Flash/RAM linker command file
* that the project has.
* The sections in the *_ZoneSelectBlock.asm source file is linked as per the commands given in the file
* NOTE - please note fill=0xFFFF, this helps if users include this file in the project by mistake and
* doesn't provide the needed proper *_ZoneSelectBlock.asm sources .
* Please refer to the Blinky DCSM example in the controlsuite examples for proper usage of this.
*
* Once users are confident that they want to program the passwords in OTP, the DSECT section type can be removed.
*
*/
MEMORY
{
PAGE 0 : /* Program Memory */
/* Z1 OTP. LinkPointers */
DCSM_OTP_Z1_LINKPOINTER : origin = 0x78000, length = 0x00000C
/* Z1 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z1_PSWDLOCK : origin = 0x78010, length = 0x000004
/* Z1 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z1_CRCLOCK : origin = 0x78014, length = 0x000004
/* Z1 OTP. RESERVED/BOOTCTRL */
DCSM_OTP_Z1_BOOTCTRL : origin = 0x7801C, length = 0x000004
/* DCSM Z1 Zone Select Contents (!!Movable!!) */
/* Z1 OTP. Z1 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z1_P0 : origin = 0x78020, length = 0x000010
DCSM_ZSEL_Z1_P1 : origin = 0x78030, length = 0x000010
DCSM_ZSEL_Z1_P2 : origin = 0x78040, length = 0x000010
DCSM_ZSEL_Z1_P3 : origin = 0x78050, length = 0x000010
DCSM_ZSEL_Z1_P4 : origin = 0x78060, length = 0x000010
DCSM_ZSEL_Z1_P5 : origin = 0x78070, length = 0x000010
DCSM_ZSEL_Z1_P6 : origin = 0x78080, length = 0x000010
DCSM_ZSEL_Z1_P7 : origin = 0x78090, length = 0x000010
DCSM_ZSEL_Z1_P8 : origin = 0x780A0, length = 0x000010
DCSM_ZSEL_Z1_P9 : origin = 0x780B0, length = 0x000010
DCSM_ZSEL_Z1_P10 : origin = 0x780C0, length = 0x000010
/* Z2 OTP. LinkPointers */
DCSM_OTP_Z2_LINKPOINTER : origin = 0x78200, length = 0x00000C
/* Z2 OTP. GPREG1/GPREG2 */
DCSM_OTP_Z2_GPREG : origin = 0x7820C, length = 0x000004
/* Z2 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z2_PSWDLOCK : origin = 0x78210, length = 0x000004
/* Z2 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z2_CRCLOCK : origin = 0x78214, length = 0x000004
/* Z2 OTP. GPREG3/BOOTCTRL */
DCSM_OTP_Z2_BOOTCTRL : origin = 0x7821C, length = 0x000004
/* DCSM Z1 Zone Select Contents (!!Movable!!) */
/* Z2 OTP. Z2 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z2_P0 : origin = 0x78220, length = 0x000010
}
SECTIONS
{
dcsm_otp_z1_linkpointer : > DCSM_OTP_Z1_LINKPOINTER PAGE = 0//, type = DSECT
dcsm_otp_z1_pswdlock : > DCSM_OTP_Z1_PSWDLOCK PAGE = 0//, type = DSECT
dcsm_otp_z1_crclock : > DCSM_OTP_Z1_CRCLOCK PAGE = 0//, type = DSECT
dcsm_otp_z1_bootctrl : > DCSM_OTP_Z1_BOOTCTRL PAGE = 0//, type = DSECT
dcsm_zsel_z1 : > DCSM_ZSEL_Z1_P0 PAGE = 0//, type = DSECT
// dcsm_zsel_z1 : > DCSM_ZSEL_Z1_P1 PAGE = 0//, type = DSECT
dcsm_otp_z2_linkpointer : > DCSM_OTP_Z2_LINKPOINTER PAGE = 0, type = DSECT
dcsm_otp_z2_pswdlock : > DCSM_OTP_Z2_PSWDLOCK PAGE = 0, type = DSECT
dcsm_otp_z2_crclock : > DCSM_OTP_Z2_CRCLOCK PAGE = 0, type = DSECT
dcsm_otp_z2_bootctrl : > DCSM_OTP_Z2_BOOTCTRL PAGE = 0, type = DSECT
dcsm_zsel_z2 : > DCSM_ZSEL_Z2_P0 PAGE = 0, type = DSECT
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
对于可能导致问题的原因、是否有任何想法? 到目前为止、我们已经克服了包括(对齐8)问题在内的所有其他问题。
本