This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28035:#10099-D 程序将无法装入可用内存,

Guru**** 667810 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1227033/tms320f28035-10099-d-program-will-not-fit-into-available-memory

器件型号:TMS320F28035

大家好

我采用这个错误

如何解决?

说明资源路径位置类型
#10099-D 程序将无法放入可用内存中,或者该段包含的调用站点需要无法为该段生成 trampoline。 对齐/分块放置在".text"大小0xe65页0的段中失败。 可用内存范围:28035_RAM_lnk.cmd /Dene line 120 C/C++ problem

我的链接器代码:

/*
// TI File $Revision: /main/2 $
// Checkin $Date: February 20, 2009   15:34:01 $
//###########################################################################
//
// FILE:    28035_RAM_lnk.cmd
//
// TITLE:   Linker Command File For 28035 examples that run out of RAM
//
//          This ONLY includes all SARAM blocks on the 28035 device.
//          This does not include flash or OTP.
//
//          Keep in mind that L0,L1,L2, and L3 are protected by the code
//          security module.
//
//          What this means is in most cases you will want to move to
//          another memory map file which has more memory defined.
//
//###########################################################################
// $TI Release: 2803x Internal Release 2 $
// $Release Date: November 11, 2008 $
//###########################################################################
*/

/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in <base>\DSP2803x_headers\cmd
//
// For BIOS applications add:      DSP2803x_Headers_BIOS.cmd
// For nonBIOS applications add:   DSP2803x_Headers_nonBIOS.cmd
========================================================= */

/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper
// locations within the memory map                                    */

/* Uncomment this line to include file only for non-BIOS applications */
/* -l DSP2803x_Headers_nonBIOS.cmd */

/* Uncomment this line to include file only for BIOS applications */
/* -l DSP2803x_Headers_BIOS.cmd */

/* 2) In your project add the path to <base>\DSP2803x_headers\cmd to the
   library search path under project->build options, linker tab,
   library search path (-i).
/*========================================================= */

/* Define the memory block start/length for the DSP2803x
   PAGE 0 will be used to organize program sections
   PAGE 1 will be used to organize data sections

   Notes:
         Memory blocks on F28035 are uniform (ie same
         physical memory) in both PAGE 0 and PAGE 1.
         That is the same memory region should not be
         defined for both PAGE 0 and PAGE 1.
         Doing so will result in corruption of program
         and/or data.

         L0 block is mirrored - that is it
         can be accessed in high memory or low memory.
         For simplicity only one instance is used in this
         linker file.

         Contiguous SARAM memory blocks can be combined
         if required to create a larger memory block.
*/

MEMORY
{
PAGE 0 :
   /* BEGIN is used for the "boot to SARAM" bootloader mode   */

   BEGIN      : origin = 0x000000, length = 0x000002
   RAMM0      : origin = 0x000050, length = 0x0003B0
   RAML0L1    : origin = 0x008000, length = 0x000C00
   RESET      : origin = 0x3FFFC0, length = 0x000002
   IQTABLES   : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2  : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
   IQTABLES3  : origin = 0x3FEBDC, length = 0x0000AA	 /* IQ Math Tables in Boot ROM */

   BOOTROM    : origin = 0x3FF27C, length = 0x000D44


PAGE 1 :

   BOOT_RSVD   : origin = 0x000002, length = 0x00004E     /* Part of M0, BOOT rom will use this for stack */
   RAMM1       : origin = 0x000480, length = 0x000380     /* on-chip RAM block M1 */
   RAML2       : origin = 0x008C00, length = 0x000400
   RAML3       : origin = 0x009000, length = 0x001000
}


SECTIONS
{
   /* Setup for "boot to SARAM" mode:
      The codestart section (found in DSP28_CodeStartBranch.asm)
      re-directs execution to the start of user code.  */
   codestart        : > BEGIN,     PAGE = 0

#ifdef __TI_COMPILER_VERSION__
   #if __TI_COMPILER_VERSION__ >= 15009000
    .TI.ramfunc : {} > RAMM0,      PAGE = 0
   #else
   ramfuncs         : > RAMM0      PAGE = 0
   #endif
#endif

   .text            : > RAML0L1,   PAGE = 0
   .cinit           : > RAMM0,     PAGE = 0
   .pinit           : > RAMM0,     PAGE = 0
   .switch          : > RAMM0,     PAGE = 0
   .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */

   .stack           : > RAMM1,     PAGE = 1
   .ebss            : > RAML2,     PAGE = 1
   .econst          : > RAML2,     PAGE = 1
   .esysmem         : > RAML2,     PAGE = 1

   IQmath           : > RAML0L1,   PAGE = 0
   IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD

  /* Uncomment the section below if calling the IQNexp() or IQexp()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {

              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

   }
   */
   /* Uncomment the section below if calling the IQNasin() or IQasin()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
   {

              IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

   }
   */

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/