This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28386D:C2000Ware 5.01.00.00 - SysConfig 器件支持

Guru**** 1130230 points
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1330682/tms320f28386d-c2000ware-5-01-00-00---sysconfig-device-support

器件型号:TMS320F28386D
主题中讨论的其他器件:SysConfigC2000WARE

大家好、

我尝试将 SysConfig 工具与 SDK C2000Ware 版本5.01.00.00一起使用、但当我添加"设备支持"时、"device.h"和"device.c"文件都生成了错误、现有的#if 大于#endif。 使用前一版本的 SDK (5.00.00.00)时不会发生这种情况。 这是某种类型的错误吗、或者我缺少其他配置吗?

感谢您的疑虑、

Ramon、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Ramon、

    请阁下观察到的错误。  如果通过 SysConfig 添加了"DeviceSupport"、则如果之前已将"device.c"和"device、h"添加到工程中、则需要排除这些内容。

    此致

    西达尔特

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Siddharth:

    SysConfig 工具为 CPU2生成的文件"device.h"和"device.c"包含错误数量的 宏#if 或#endif、很容易重现:

    然后、添加器件支持、SysConfig 生成的文件将为:

    //#############################################################################
    //
    // FILE:   device.c
    //
    // TITLE:  Device setup for examples.
    //
    //#############################################################################
    /*
    * Copyright (c) 2020 Texas Instruments Incorporated - http://www.ti.com
    * All rights reserved.
    *
    * Redistribution and use in source and binary forms, with or without
    * modification, are permitted provided that the following conditions
    * are met:
    *
    * *  Redistributions of source code must retain the above copyright
    *    notice, this list of conditions and the following disclaimer.
    *
    * *  Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the
    *    documentation and/or other materials provided with the distribution.
    *
    * *  Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
    * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
    * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
    * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
    * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
    * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
    * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
    * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
    * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
    * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
    * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    */  
    //#############################################################################
    
    //
    // Included Files
    //
    #include "device.h"
    #include "board.h"
    #include "clocktree.h"
    
    #ifdef CMDTOOL
    #include "device_cmd.h"
    #endif
    
    //*****************************************************************************
    //
    // Function to initialize the device. Primarily initializes system control to a
    // known state by disabling the watchdog, setting up the SYSCLKOUT frequency,
    // and enabling the clocks to the peripherals.
    //
    //*****************************************************************************
    void Device_init(void)
    {
        //
        // Disable the watchdog
        //
        SysCtl_disableWatchdog();
    #ifdef CMDTOOL
        CMD_init();
    #endif
    
    #ifdef _FLASH
    #ifndef CMDTOOL
        //
        // Copy time critical code and flash setup code to RAM. This includes the
        // following functions: InitFlash();
        //
        // The RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart symbols
        // are created by the linker. Refer to the device .cmd file.
        //
        memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
    #endif
        //
        // Call Flash Initialization to setup flash waitstates. This function must
        // reside in RAM.
        //
        Flash_initModule(FLASH0CTRL_BASE, FLASH0ECC_BASE, DEVICE_FLASH_WAITSTATES);
    #endif
    #ifdef CPU1
        //
        // Verify the crystal frequency.
        // Note: This check can be removed if you are not using XTAL as the PLL
        // source
        //
        if( ((DEVICE_SETCLOCK_CFG & SYSCTL_OSCSRC_M) == SYSCTL_OSCSRC_XTAL) ||
            ((DEVICE_SETCLOCK_CFG & SYSCTL_OSCSRC_M) == SYSCTL_OSCSRC_XTAL_SE))
        {
            if(!Device_verifyXTAL(DEVICE_OSCSRC_FREQ / 1000000))
            {
                //
                // The actual XTAL frequency does not match DEVICE_OSCSRC_FREQ!!
                // Please check the XTAL frequency used.
                //
                // By default, the Device_init function assumes 25MHz XTAL.
                // If a 20MHz crystal is used, please add a predefined symbol
                // "USE_20MHZ_XTAL" in your CCS project.
                // If a different XTAL is used, please update the DEVICE_SETCLOCK_CFG
                // macro accordingly.
                //
                // Note that the latest F2838x controlCARDs (Rev.B and later) have been
                // updated to use 25MHz XTAL by default. If you have an older 20MHz XTAL
                // controlCARD (E1, E2, or Rev.A), refer to the controlCARD
                // documentation on steps to reconfigure the controlCARD from 20MHz to
                // 25MHz.
                //
                ESTOP0;
                while(1);
            }
        }
        
    #endif
    
        Device_initGPIO();  
    }
    
    //*****************************************************************************
    //
    // Function to turn on all peripherals, enabling reads and writes to the
    // peripherals' registers.
    //
    // Note that to reduce power, unused peripherals should be disabled.
    //
    //*****************************************************************************
    void Device_enableAllPeripherals(void)
    {
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLA1);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DMA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TIMER0);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TIMER1);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TIMER2);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CPUBGCRC);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLA1BGCRC);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_HRCAL);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ERAD);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM1);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM2);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM3);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM4);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM5);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM6);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM7);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM8);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM9);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM10);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM11);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM12);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM13);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM14);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM15);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM16);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP1);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP2);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP3);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP4);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP5);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP6);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP7);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EQEP1);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EQEP2);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EQEP3);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SD1);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SD2);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCIA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCIB);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCIC);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCID);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SPIA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SPIB);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SPIC);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SPID);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_I2CA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_I2CB);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CANA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CANB);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_MCANA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_MCBSPA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_MCBSPB);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCB);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCC);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCD);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS1);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS2);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS3);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS4);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS5);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS6);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS7);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS8);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DACA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DACB);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DACC);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLB1);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLB2);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLB3);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLB4);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLB5);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLB6);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLB7);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLB8);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSITXA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSITXB);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSIRXA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSIRXB);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSIRXC);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSIRXD);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSIRXE);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSIRXF);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSIRXG);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_FSIRXH);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_PMBUSA);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DCC0);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DCC1);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DCC2);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_MPOSTCLK);
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAT);
    }
    
    //*****************************************************************************
    //
    // Function to disable pin locks and enable pullups on GPIOs.
    //
    //*****************************************************************************
    void Device_initGPIO(void)
    {
        //
        // Disable pin locks.
        //
        GPIO_unlockPortConfig(GPIO_PORT_A, 0xFFFFFFFF);
        GPIO_unlockPortConfig(GPIO_PORT_B, 0xFFFFFFFF);
        GPIO_unlockPortConfig(GPIO_PORT_C, 0xFFFFFFFF);
        GPIO_unlockPortConfig(GPIO_PORT_D, 0xFFFFFFFF);
        GPIO_unlockPortConfig(GPIO_PORT_E, 0xFFFFFFFF);
        GPIO_unlockPortConfig(GPIO_PORT_F, 0xFFFFFFFF);
    
        //
        // Enable GPIO Pullups
        //
        Device_enableUnbondedGPIOPullups();
    }
    
    //*****************************************************************************
    //
    // Function to enable pullups for the unbonded GPIOs on the 176PTP package:
    // GPIOs     Grp Bits
    // 95-132    C   31
    //           D   31:0
    //           E   4:0
    // 134-168   E   31:6
    //           F   8:0
    //
    //*****************************************************************************
    
    void Device_enableUnbondedGPIOPullupsFor176Pin(void)
    {
    
        EALLOW;
        HWREG(GPIOCTRL_BASE + GPIO_O_GPCPUD) = ~0x80000000U;
        HWREG(GPIOCTRL_BASE + GPIO_O_GPDPUD) = ~0xFFFFFFF7U;
        HWREG(GPIOCTRL_BASE + GPIO_O_GPEPUD) = ~0xFFFFFFDFU;
        HWREG(GPIOCTRL_BASE + GPIO_O_GPFPUD) = ~0x000001FFU;
        EDIS;
    }
    
    //*****************************************************************************
    //
    // Function to enable pullups for the unbonded GPIOs on the
    // 176PTP package.
    //
    //*****************************************************************************
    void Device_enableUnbondedGPIOPullups(void)
    {
        //
        // bits 8-10 have pin count
        //
        uint16_t pinCount = ((HWREG(DEVCFG_BASE + SYSCTL_O_PARTIDL) &
                              (uint32_t)SYSCTL_PARTIDL_PIN_COUNT_M) >>
                             SYSCTL_PARTIDL_PIN_COUNT_S);
    
        /*
         * 6 = 176 pin
         * 7 = 337 pin
         */
        if (pinCount == 6)
        {
            Device_enableUnbondedGPIOPullupsFor176Pin();
        }
        else
        {
            //
            // Do nothing - this is 337 pin package
            //
        }
    }
    
    
    //*****************************************************************************
    //
    // Function to verify the XTAL frequency
    // freq is the XTAL frequency in MHz
    // The function return true if the the actual XTAL frequency matches with the
    // input value
    //
    // Note that this function assumes that the PLL is not already configured and
    // hence uses SysClk freq = 10MHz for DCC calculation
    //
    //*****************************************************************************
    #ifdef CPU1
    bool Device_verifyXTAL(float freq)
    {
        //
        // Use DCC to verify the XTAL frequency using INTOSC2 as reference clock
        //
    
        //
        // Enable DCC0 clock
        //
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DCC0);
    
        //
        // Insert atleast 5 cycles delay after enabling the peripheral clock
        //
        asm(" RPT #5 || NOP");
    
        //
        // Configures XTAL as CLKSRC0 and INTOSC2 as CLKSRC1
        // Fclk0 = XTAL frequency (input parameter)
        // Fclk1 = INTOSC2 frequency = 10MHz
        //
        // Configuring DCC error tolerance of +/-1%
        // INTOSC2 can have a variance in frequency of +/-10%
        //
        // Assuming PLL is not already configured, SysClk freq = 10MHz
        //
        // Note : Update the tolerance and INTOSC2 frequency variance as necessary.
        //
        return (DCC_verifyClockFrequency(DCC0_BASE,
                                         DCC_COUNT1SRC_INTOSC2, 10.0F,
                                         DCC_COUNT0SRC_XTAL, freq,
                                         1.0F, 10.0F, 10.0F));
    
    }
    #endif
    
    
    
    //*****************************************************************************
    //
    // Function to boot CM
    // Available bootmodes :
    //      - BOOTMODE_BOOT_TO_FLASH_SECTOR0
    //      - BOOTMODE_BOOT_TO_FLASH_SECTOR4
    //      - BOOTMODE_BOOT_TO_FLASH_SECTOR8
    //      - BOOTMODE_BOOT_TO_FLASH_SECTOR13
    //      - BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR0
    //      - BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR4
    //      - BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR8
    //      - BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR13
    //      - BOOTMODE_IPC_MSGRAM_COPY_BOOT_TO_S0RAM
    //      - BOOTMODE_BOOT_TO_S0RAM
    //      - BOOTMODE_BOOT_TO_USEROTP
    //
    // Note that while using BOOTMODE_IPC_MSGRAM_COPY_BOOT_TO_M1RAM,
    // BOOTMODE_IPC_MSGRAM_COPY_LENGTH_xxxW must be ORed with the bootmode parameter
    //
    // This function must be called after Device_init function
    //
    //*****************************************************************************
    void Device_bootCM(uint32_t bootmode)
    {
        //
        // Configure the CPU1TOCMIPCBOOTMODE register
        //
        IPC_setBootMode(IPC_CPU1_L_CM_R,
                        (BOOT_KEY | CM_BOOT_FREQ_125MHZ | bootmode));
    
        //
        // Set IPC Flag 0
        //
        IPC_setFlagLtoR(IPC_CPU1_L_CM_R, IPC_FLAG0);
    
        //
        // Bring CM out of reset. Wait for CM to go out of reset.
        //
        SysCtl_controlCMReset(SYSCTL_CORE_DEACTIVE);
        while(SysCtl_isCMReset() == 0x1U);
    }
    #endif
    
    //*****************************************************************************
    //
    // Error handling function to be called when an ASSERT is violated
    //
    //*****************************************************************************
    void __error__(const char *filename, uint32_t line)
    {
        //
        // An ASSERT condition was evaluated as false. You can use the filename and
        // line parameters to determine what went wrong.
        //
        ESTOP0;
    }
    
    

    以及:

    //#############################################################################
    //
    // FILE:   device.h
    //
    // TITLE:  Device setup for examples.
    //
    //#############################################################################
    //
    // Copyright (C) 2014-2022 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //#############################################################################
    #ifndef __DEVICE_H__
    #define __DEVICE_H__
    //
    // Included Files
    //
    #include "driverlib.h"
    #include "clocktree.h"
    
    #if (!defined(CPU1) && !defined(CPU2))
    #error "You must define CPU1 or CPU2 in your project properties.  Otherwise, \
    the offsets in your header files will be inaccurate."
    #endif
    
    #if (defined(CPU1) && defined(CPU2))
    #error "You have defined both CPU1 and CPU2 in your project properties.  Only \
    a single CPU should be defined."
    #endif
    
    
    //*****************************************************************************
    //
    // Macro to call SysCtl_delay() to achieve a delay in microseconds. The macro
    // will convert the desired delay in microseconds to the count value expected
    // by the function. \b x is the number of microseconds to delay.
    //
    //*****************************************************************************
    #define DEVICE_DELAY_US(x) SysCtl_delay(((((long double)(x)) / (1000000.0L /  \
                                    (long double)DEVICE_SYSCLK_FREQ)) - 9.0L) / 5.0L)
    
    //*****************************************************************************
    //
    // Macros related to booting CPU2 and CM. These can be used while invoking the
    // functions Device_bootCPU2() and Device_bootCM(). 
    //
    // Note that the macros CM_BOOT_FREQ_125MHZ and CPU2_BOOT_FREQ_200MHZ are used
    // in the functions Device_bootCM() and Device_bootCPU2() respectively. Please
    // update the function and the macros if you are using a different clock
    // frequency.
    //
    //*****************************************************************************
    #ifdef CPU1
    #define BOOT_KEY                                0x5A000000UL
    #define CM_BOOT_FREQ_125MHZ                     0x7D00U
    #define CPU2_BOOT_FREQ_200MHZ                   0xC800U
    
    #define BOOTMODE_BOOT_TO_FLASH_SECTOR0          0x03U
    #define BOOTMODE_BOOT_TO_FLASH_SECTOR4          0x23U
    #define BOOTMODE_BOOT_TO_FLASH_SECTOR8          0x43U
    #define BOOTMODE_BOOT_TO_FLASH_SECTOR13         0x63U
    #define BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR0   0x0AU
    #define BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR4   0x2AU
    #define BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR8   0x4AU
    #define BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR13  0x6AU
    #define BOOTMODE_IPC_MSGRAM_COPY_BOOT_TO_M1RAM  0x0CU
    #define BOOTMODE_IPC_MSGRAM_COPY_BOOT_TO_S0RAM  0x0CU
    #define BOOTMODE_BOOT_TO_M0RAM                  0x05U
    #define BOOTMODE_BOOT_TO_S0RAM                  0x05U
    #define BOOTMODE_BOOT_TO_USEROTP                0x0BU
    
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_100W    0x10000U
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_200W    0x20000U
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_300W    0x30000U
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_400W    0x40000U
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_500W    0x50000U
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_600W    0x60000U
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_700W    0x70000U
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_800W    0x80000U
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_900W    0x90000U
    #define BOOTMODE_IPC_MSGRAM_COPY_LENGTH_1000W   0xA0000U
    #endif
    
    //*****************************************************************************
    //
    // Defines, Globals, and Header Includes related to Flash Support
    //
    //*****************************************************************************
    #ifdef _FLASH
    #include <stddef.h>
    
    #ifndef CMDTOOL
    extern uint16_t RamfuncsLoadStart;
    extern uint16_t RamfuncsLoadEnd;
    extern uint16_t RamfuncsLoadSize;
    extern uint16_t RamfuncsRunStart;
    extern uint16_t RamfuncsRunEnd;
    extern uint16_t RamfuncsRunSize;
    #endif
    
    #define DEVICE_FLASH_WAITSTATES 3
    
    #endif
    
    //*****************************************************************************
    //
    // Function Prototypes
    //
    //*****************************************************************************
    //*****************************************************************************
    //
    //! \addtogroup device_api
    //! @{
    //
    //*****************************************************************************
    //*****************************************************************************
    //
    //! Function to initialize the device. Primarily initializes system 
    //! control to a known state by disabling the watchdog, setting up the
    //! SYSCLKOUT frequency, and enabling the clocks to the peripherals.
    //!
    //! \param None.
    //! \return None.
    //
    //*****************************************************************************
    extern void Device_init(void);
    
    
    //*****************************************************************************
    //!
    //!
    //! @brief Function to turn on all peripherals, enabling reads and writes to the
    //! peripherals' registers.
    //!
    //! Note that to reduce power, unused peripherals should be disabled.
    //!
    //! @param None
    //! @return None
    //
    //*****************************************************************************
    extern void Device_enableAllPeripherals(void);
    //*****************************************************************************
    //!
    //!
    //! @brief Function to disable pin locks on GPIOs.
    //!
    //! @param None
    //! @return None
    //
    //*****************************************************************************
    extern void Device_initGPIO(void);
    
    //*****************************************************************************
    //!
    //! @brief Function to enable pullups for the unbonded GPIOs on the 176PTP package:
    //! GPIOs     Grp Bits
    //! 95-132    C   31
    //!           D   31:0
    //!           E   4:0
    //! 134-168   E   31:6
    //!           F   8:0
    //!
    //! @param None
    //! @return None
    //
    //*****************************************************************************
    extern void Device_enableUnbondedGPIOPullupsFor176Pin(void);
    //*****************************************************************************
    //!
    //! @brief Function to enable pullups for the unbonded GPIOs on the
    //! 176PTP package.
    //!
    //! @param None
    //! @return None
    //
    //*****************************************************************************
    extern void Device_enableUnbondedGPIOPullups(void);
    
    
    
    //*****************************************************************************
    //
    //! @brief Function to boot CM
    //!
    //! \param bootmode is the mode in which CM should boot.
    //!
    //! Available bootmodes :
    //!      - BOOTMODE_BOOT_TO_FLASH_SECTOR0
    //!      - BOOTMODE_BOOT_TO_FLASH_SECTOR4
    //!      - BOOTMODE_BOOT_TO_FLASH_SECTOR8
    //!      - BOOTMODE_BOOT_TO_FLASH_SECTOR13
    //!      - BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR0
    //!      - BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR4
    //!      - BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR8
    //!      - BOOTMODE_BOOT_TO_SECURE_FLASH_SECTOR13
    //!      - BOOTMODE_IPC_MSGRAM_COPY_BOOT_TO_S0RAM
    //!      - BOOTMODE_BOOT_TO_S0RAM
    //!      - BOOTMODE_BOOT_TO_USEROTP
    //!
    //! Note that while using BOOTMODE_IPC_MSGRAM_COPY_BOOT_TO_M1RAM,
    //! BOOTMODE_IPC_MSGRAM_COPY_LENGTH_xxxW must be ORed with the bootmode parameter
    //!
    //! This function must be called after Device_init function
    //! \return None.
    //
    //*****************************************************************************
    extern void Device_bootCM(uint32_t bootmode);
    
    //*****************************************************************************
    //
    //!
    //! @brief Function to verify the XTAL frequency
    //! \param freq is the XTAL frequency in MHz
    //! \return The function return true if the the actual XTAL frequency matches with the
    //! input value
    //
    //*****************************************************************************
    extern bool Device_verifyXTAL(float freq);
    #endif
    
    //*****************************************************************************
    //!
    //! @brief Error handling function to be called when an ASSERT is violated
    //!
    //! @param *filename File name in which the error has occurred
    //! @param line Line number within the file
    //! @return None
    //
    //*****************************************************************************
    extern void __error__(const char *filename, uint32_t line);
    //*****************************************************************************
    //
    // Close the Doxygen group.
    //! @}
    //
    //*****************************************************************************
    #endif // __DEVICE_H__
    

    此文件有错误(宏#if 和#endif 的数量不匹配)。

    是一个错误、还是我做错了什么?

    感谢您的回复。

    拉蒙

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Ramon。

    这看起来像是一个错误、会将其报告给开发团队

    此致

    西达尔特