This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28377S:Tms320f28377s 在闪存 API 中非法 ısr μ s

Guru**** 2468460 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1424621/tms320f28377s-tms320f28377s-illegal-sr-in-flash-api

器件型号:TMS320F28377S

工具与软件:

大家好、

我想使用闪存 API 将它写入处理器的闪存并擦除我自己的代码、但它在调试屏幕中进入了非法 ISR、我不知道为什么、您可以看到链接器文件和下面代码的相关部分、问题的来源是什么

MEMORY
{
PAGE 0 :  /* Program Memory */
          /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
//   BEGIN           	: origin = 0x080000, length = 0x000002
   RAMM0           	: origin = 0x000122, length = 0x0002DE
   RAMD0           	: origin = 0x00B000, length = 0x000800
   RAMLS0          	: origin = 0x008000, length = 0x000800
   RAMLS1          	: origin = 0x008800, length = 0x000800
   RAMLS2      		: origin = 0x009000, length = 0x000800
   RAMLS3      		: origin = 0x009800, length = 0x000800
   RAMLS4      		: origin = 0x00A000, length = 0x000800
   RAMGS14     		: origin = 0x01A000, length = 0x001000
   RAMGS15     		: origin = 0x01B000, length = 0x001000
   RESET           	: origin = 0x3FFFC0, length = 0x000002

#ifdef __TI_COMPILER_VERSION__
   #if __TI_COMPILER_VERSION__ >= 20012000
GROUP {      /* GROUP memory ranges for crc/checksum of entire flash */
   #endif
#endif

    /* BEGIN is used for the "boot to Flash" bootloar mode   */

	BEGIN           	: origin = 0x080000, length = 0x000002
	/* Flash sectors */
   FLASHA           : origin = 0x080002, length = 0x001FFE	/* on-chip Flash */
   FLASHB           : origin = 0x082000, length = 0x002000	/* on-chip Flash */
   FLASHC           : origin = 0x084000, length = 0x002000	/* on-chip Flash */
   FLASHD           : origin = 0x086000, length = 0x002000	/* on-chip Flash */
   FLASHE           : origin = 0x088000, length = 0x008000	/* on-chip Flash */
   FLASHF           : origin = 0x090000, length = 0x008000	/* on-chip Flash */
   FLASHG           : origin = 0x098000, length = 0x008000	/* on-chip Flash */
   FLASHH           : origin = 0x0A0000, length = 0x008000	/* on-chip Flash */
   FLASHI           : origin = 0x0A8000, length = 0x008000	/* on-chip Flash */
   FLASHJ           : origin = 0x0B0000, length = 0x008000	/* on-chip Flash */
   FLASHK           : origin = 0x0B8000, length = 0x002000	/* on-chip Flash */
   FLASHL           : origin = 0x0BA000, length = 0x002000	/* on-chip Flash */
   FLASHM           : origin = 0x0BC000, length = 0x002000	/* on-chip Flash */
   FLASHN           : origin = 0x0BE000, length = 0x002000	/* on-chip Flash */

//   FLASHN_RSVD     : origin = 0x0BFFF0, length = 0x000010    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

#ifdef __TI_COMPILER_VERSION__
  #if __TI_COMPILER_VERSION__ >= 20012000
}  crc(_ccs_flash_checksum, algorithm=C28_CHECKSUM_16)
  #endif
#endif

PAGE 1 : /* Data Memory */
         /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

   BOOT_RSVD       : origin = 0x000002, length = 0x000120     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAMD1           : origin = 0x00B800, length = 0x000800

   RAMLS5      : origin = 0x00A800, length = 0x000800

   RAMGS0      : origin = 0x00C000, length = 0x001000
   RAMGS1      : origin = 0x00D000, length = 0x001000
   RAMGS2      : origin = 0x00E000, length = 0x001000
   RAMGS3      : origin = 0x00F000, length = 0x001000
   RAMGS4      : origin = 0x010000, length = 0x001000
   RAMGS5      : origin = 0x011000, length = 0x001000
   RAMGS6      : origin = 0x012000, length = 0x001000
   RAMGS7      : origin = 0x013000, length = 0x001000

}


SECTIONS
{
   /* Allocate program areas: */
   .cinit              						: > FLASHB | FLASHC     PAGE = 0, ALIGN(8)
   .pinit              						: > FLASHB,     PAGE = 0, ALIGN(8)
   .text:Fapi_issueAsyncCommandWithAddress	: {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_checkFsmForReady				: {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_doBlankCheck					: {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_issueProgrammingCommand		: {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_getFsmStatus					: {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_doVerify					    : {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_setActiveFlashBank			: {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_issueAsyncCommandWithAddress	: {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_initializeAPI				    : {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_isAddressEcc				    : {} LOAD = FLASHA, RUN = RAMGS0
   .text:Fapi_serviceWatchdogTimer		    : {} LOAD = FLASHA, RUN = RAMGS0
   .text:Example_FlashProgram				: {} LOAD = FLASHA, RUN = RAMGS0
   .text               						: > FLASHI      PAGE = 0, ALIGN(8)
   codestart           						: > BEGIN       PAGE = 0, ALIGN(8)

#ifdef __TI_COMPILER_VERSION__
   #if __TI_COMPILER_VERSION__ >= 15009000
        #if defined(__TI_EABI__)
            .TI.ramfunc : {} LOAD = FLASHA,
                                 RUN = RAMLS0,
                                 LOAD_START(RamfuncsLoadStart),
                                 LOAD_SIZE(RamfuncsLoadSize),
                                 LOAD_END(RamfuncsLoadEnd),
                                 RUN_START(RamfuncsRunStart),
                                 RUN_SIZE(RamfuncsRunSize),
                                 RUN_END(RamfuncsRunEnd),
		                         PAGE = 0, ALIGN(8)
         #endif
   #endif
#endif

   /* Allocate uninitalized data sections: */
   .stack              : > RAMM1        PAGE = 1
   .init_array         : > FLASHB,       PAGE = 0,       ALIGN(8)
   .bss                : > RAMLS5,       PAGE = 1
   .ebss               : >> RAMLS5 | RAMGS0 | RAMGS1      PAGE = 1
   .esysmem            : > RAMLS5       PAGE = 1
   .data               : >> RAMLS5 | RAMGS1 ,       PAGE = 1, ALIGN(8)
   .sysmem             : > RAMLS5,       PAGE = 1
   .const              : > FLASHF,       PAGE = 0,       ALIGN(8)

   /* Initalized sections go in Flash */
   .econst             : >> FLASHF | FLASHG      PAGE = 0, ALIGN(8)
   .switch             : > FLASHD      PAGE = 0, ALIGN(8)

   .reset              : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
  Filter_RegsFile     : > RAMGS0,	   PAGE = 1

   SHARERAMGS0		: > RAMGS0,		PAGE = 1
   SHARERAMGS1		: > RAMGS1,		PAGE = 1

   /* Flash Programming Buffer */
   BufferDataSection : > RAMD1, PAGE = 1, ALIGN(8)
   /* crc/checksum section configured as COPY section to avoid including in executable */
  .TI.memcrc          : type = COPY

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

        }


    }

extern Fapi_StatusType Fapi_initializeAPI(
                                         Fapi_FmcRegistersType *poFlashControlRegister,
                                         uint32 u32HclkFrequency
                                         );


extern Fapi_StatusType Fapi_setActiveFlashBank(Fapi_FlashBankType oFlashBank);

extern Fapi_StatusType Fapi_issueAsyncCommandWithAddress(
                                                        Fapi_FlashStateCommandsType oCommand,
                                                        uint32 *pu32StartAddress
                                                        );
void Example_FlashProgram(Uint16 data)
{
    Fapi_StatusType oReturnCheck;
    Fapi_FlashStatusWordType oFlashStatusWord;

    EALLOW;

    PUMPREQUEST = 0x5A5A0002;

    oReturnCheck = Fapi_initializeAPI(F021_CPU0_W0_BASE_ADDRESS, 200);
    if (oReturnCheck != Fapi_Status_Success) {
        //Example_Error(oReturnCheck);
    }

    oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);
    if (oReturnCheck != Fapi_Status_Success) {
        //Example_Error(oReturnCheck);
    }


    oReturnCheck = Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector, (Uint32 *)FLASH_SECTOR_START);
    while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady) {}


    oReturnCheck = Fapi_doBlankCheck((Uint32 *)FLASH_SECTOR_START, FLASH_SECTOR_LENGTH, &oFlashStatusWord);
    if (oReturnCheck != Fapi_Status_Success) {
       // Example_Error(oReturnCheck);
    }


    oReturnCheck = Fapi_issueProgrammingCommand((Uint32 *)FLASH_SECTOR_START, &data, 1, 0, 0, Fapi_AutoEccGeneration);
    while (Fapi_checkFsmForReady() == Fapi_Status_FsmBusy) {}

    if (oReturnCheck != Fapi_Status_Success) {
        //Example_Error(oReturnCheck);
    }

    EDIS;
}


Uint32 Example_FlashRead(void)
{

    value_read = *(Uint32 *)FLASH_SECTOR_START;
    return value_read;
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您能否检查您的映射文件以确认闪存 API 已复制到 RAM?

    谢谢、此致、

    Rajeshwary