This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMK5C33414A:VCO3 频率容差

Guru**** 2680595 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/1575084/lmk5c33414a-vco3-frequency-tolerance

器件型号:LMK5C33414A


工具/软件:

您好 TI、

所有类似的 2457.6MHz 和 2500MHz 器件都具有±0.01%的 BAW 容差、但该容差指定为±1%:

是否还应将其指定为±0.01%?