在此过程中,6.8GHz信号的输出频率没有问题。 修改输出频率时,仅修改R44和R0寄存器,其中reg44_data更改约1位,频谱将看到瞬时闪烁。
如果输出频率更改为120Hz (600Hz频率跳频约为6.8G),则会出现大量伪频率。
我想问一下,修改十进制N分频器瞬时噪声是锁相环的固有特征吗? 是否有办法消除或减少这种现象?
修改输出频率时,仅修改R44和R0寄存器,其中reg44_data更改约8位。
WriteOneByte (reg44_data);//R44,reg44_data=0x2CAC1A;
WriteOneByte (0x0.0227万C);//R0
设备初始为以下参数:
WriteOneByte (0x4000AF);//R64
WriteOneByte (0x3E0000);//R62
WriteOneByte (0x3D0001);//R61
WriteOneByte (0x3B0000);//R59
WriteOneByte (0x3003FD);//R48
WriteOneByte (0x2F08CF);//R47
WriteOneByte (0x2E38A2);//R46
WriteOneByte (0x2D36E2);//R45
WriteOneByte (0x2CAC1A);//R44
WriteOneByte (0x2B0000);//R43
WriteOneByte (0x2A0000);//R42
WriteOneByte (0x29FFFF);//R41
WriteOneByte (0x28FFFF);//R40
WriteOneByte (0x27.8204万);//R39
WriteOneByte (0x260D58);//R38
WriteOneByte (0x25.5万);//R37
WriteOneByte (0x24.0401万);//R36
WriteOneByte (0x23.0219万);//R35
WriteOneByte (0x22C3D0);//R34
WriteOneByte (0x21.421万);//R33
WriteOneByte (0x20.421万);//R32
WriteOneByte (0x1F0401);//R31
WriteOneByte (0x1E0034);//R30
WriteOneByte (0x1D0084);//R29
WriteOneByte (0x1C2924);//R28
WriteOneByte (0x19万);//R25
WriteOneByte (0x18.0509万);//R24
WriteOneByte (0x17.8842万);//R23
WriteOneByte (0x16.23万);//R22
WriteOneByte (0x1.4012万C);//R20
WriteOneByte (0x13.0965万);//R19
WriteOneByte (0x0E0F7B);//R14
WriteOneByte (0x0D4000);//R13
WriteOneByte (0x0C7014);//R12
WriteOneByte (0x0B0028);//R11
WriteOneByte (0x0A10D8);//R10
WriteOneByte (0x090B02);//R9
WriteOneByte (0x8.1084万);//R8
WriteOneByte (0x0728B2);//R7
WriteOneByte (0x4.1943万);//R4
WriteOneByte (0x2.05万);//R2
WriteOneByte (0x1.0808万);//R1
WriteOneByte (0x0.0227万C);//R0