请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LMX2594 您好,
如果FPD=10MHz,RAPK_LIMIT功能会将斜坡范围限制在+/-2.56GHz范围内,并且fvco无法覆盖整个7.5GHz至15GHz频率范围。 正确吗?
是否可以禁用RAPK_LIMIT功能?
谢谢!
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
如果FPD=10MHz,RAPK_LIMIT功能会将斜坡范围限制在+/-2.56GHz范围内,并且fvco无法覆盖整个7.5GHz至15GHz频率范围。 正确吗?
是否可以禁用RAPK_LIMIT功能?
谢谢!
John