请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:CDCM7005 您好,
我在电子主板上使用CDCM7005,两个REF_CLK (10MHz)和一个VCXO (960MHz)。
我的配置如下:
当我将REF_CLK引脚(QFN中为35)驱动到'1'以使用PRI_REF切换时,CDCM不会切换到主时钟(PLL在SEC_REF上锁定)。
为什么?
感谢您的回复,
Sebastien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.